This forum is for engineers working EcoStruxure Building Operation, wanting to leverage the SEAL application to improve the efficiency in the engineering process.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-2301:24 PM
I'll reply with a question... 🙂 Do you have an example graphic that is not working in EBO 2025 due to this?
On a side note, it's a topic which is a bit more serious than it was maybe anticipated by LoB. It's something we'll need to have further discussions on. We know that the requirement of not using these will not go away, and know that some things will probably be handled in SEAL... and then there's the "TGML Search and Replace". You'll see that I've already posted an update including a fix for the "Curve" component from the Community which used the StringBuilder.
So long story short:
1. I'd like to see concrete examples you have of graphics not working in 7.0
2. The topic is something we're looking at in a wider perspective