Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
This forum is for engineers working EcoStruxure Building Operation, wanting to leverage the SEAL application to improve the efficiency in the engineering process.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-01-22 07:04 AM . Last Modified: 2025-01-22 09:56 PM
Duplicate and rename is a script that creates a copy of content (source) and puts it in a specified location (target). In that same process, the duplicated content can be renamed and potential existing content that exists in the target location can be replaced. Simply put, it's a flexible combination of mass duplication, mass distribution and mass alteration or replacement of content where one does not necessarily exclude or depend on the other. This will have profound impact on engineering-efficiency related to producing or modifying content.
The duplication part creates copies of one or multiple objects, folders with underlying content, controllers, devices, etc. The rename part then modifies the name of those objects, their BACnet name property or even content inside graphics intrinsic to their source based on file input. Finally, the replace part swaps content that already exists with new content. This can either be done sequentially in one execution or iterated over time in multiple runs.
It is important to emphasize that the script operates in a left to right order in regards to arranging colums properly. Each row represents a source to duplicate to a target and rename. Any field that is left empty will be ignored.
Creating lists of paths pointing to sources and targets can easily be built by performing searches and copying the results into the CSV-file.
Example 1:
Using two controllers (RP-C) with different configurations as a template to distribute multiple copies with unique application-specific names.
| Column A | Column B | Column C | Column D | Column E | Column F | |
| Row 1 | Source | Target | Target Name | APP1- | RmTmp | SaDpr |
| Row 2 | /AS/BACnet Interface/IP Network/RPC_01 | /AS/BACnet Interface/IP Network | R101 | R101- | RmTmp101 | SaDpr101 |
| Row 3 | /AS/BACnet Interface/IP Network/RPC_02 | /AS/BACnet Interface/IP Network | R102 | R102- | RmTmp102 | SaDpr102 |
| Row 4 | /AS/BACnet Interface/IP Network/RPC_02 | /AS/BACnet Interface/IP Network | R103 | R103- | RmTmp103 | SaDpr103 |
Example 2:
Using one controller (RP-C) as a template to distribute multiple copies with unique application-specific names that contains a prefix.
| Column A | Column B | Column C | Column D | Column E | |
| Row 1 | Source | Target | Target Name | APP1-HtgVlv | APP1-ClgVlv |
| Row 2 | /AS/BACnet Interface/IP Network/MPC_03 | /AS/BACnet Interface/IP Network | R104 | AHU1-HtgVlv1 | AHU1-ClgVlv1 |
| Row 3 | /AS/BACnet Interface/IP Network/MPC_03 | /AS/BACnet Interface/IP Network | R105 | AHU1-HtgVlv2 | AHU1-ClgVlv2 |
| Row 4 | /AS/BACnet Interface/IP Network/MPC_03 | /AS/BACnet Interface/IP Network | R106 | AHU1-HtgVlv3 | AHU1-ClgVlv3 |
Example 3:
Using one Modbus device as a template to create multiple copies with unique device names where the underlying content is not renamed.
| Column A | Column B | Column C | Column D | |
| Row 1 | Source | Target | Target Name | |
| Row 2 | /AS/Modbus Master Network/VAV | /AS/BACnet Interface/IP Network\RPC_04\IO Resources\Modbus | AHU1-VavSaDpr4 | |
| Row 3 | /AS/Modbus Master Network/VAV | /AS/BACnet Interface/IP Network\RPC_05\IO Resources\Modbus | AHU1-VavSaDpr5 | |
| Row 4 | /AS/Modbus Master Network/VAV | /AS/BACnet Interface/IP Network\RPC_06\IO Resources\Modbus | AHU1-VavSaDpr6 |
This specifies what to do if any content with identical name already exists in the specified target path for the duplicated object name. Content can either be duplicated, distributed and replaced simultaneously in one run.
Replace will remove any existing content located in the target path and replace it with the content specified in the source path, allowing for scenarios like updating og re-distributing content that contains slight modifications to what currently exists in the target path. Skip will simply pass on each instance where content specified in the target path already exists and move on to the next item in the list. Stop will halt at the first instance where content specified in the target path already exists so it can be manually inspected.
Narrow or widen the scope by filtering what type of objects can be affected. Any object type not selected will be excluded from being renamed. Please note that Segment values is unchecked by default, as any changes to the name property for segment objects need to be done carefully in order not to make incidental alterations to combined segments set by rezoning as their naming needs to be intact in order to match and function properly.
Due to the nature of the script the Name property is always processed. However, the BACnet Name property can either be included or excluded from being renamed.
Container objects are bodies that contain runtime objects with a set of properties and logic. Any content stored inside these objects that matches the specified strings by name will be replaced.
Bound values are kept intact by taking by making sure the bind path reflects any change done if an object is renamed, meaning database content can be excessively altered without resulting in deterioration.
The advantage of being able to replace content of container objects at the same time as other objects and their properties elsewhere in the database while simultaneously keeping any bindings intact so they are not lost when renaming has the potential of increasing the time-efficiency compared to doing this manually by several orders of magnitude.
The Duplicate & Rename Script is one of our standard script available in the Standard tab when using the SEAL Script utility.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-01 11:55 AM
Hi!
I would like to use this tool to duplicate and rename the content of a graphic. I filled up the .csv and executed the script on my template graphic, but in the result graphic there is no template texts renamed, the script did not modify any of the texts written in the first row of the .csv. Attached my template graphic, result graphic, csv and execution log. (I checked all the checkboxes in SEAL parameters and the script renamed correctly the Graphic, but did not do anything inside of it). Thank you for your help!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-01 10:38 PM
Nice Script 👍
I just saw the line
| /AS/Modbus Master Network/VAV | /AS/BACnet Interface/IP Network\RPC_04\IO Resources\Modbus |
and I was thinking RP-C. Is it possible to copy Modbus point from a AS to RP-C with the new script ? 😃
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-02 12:02 AM
I published a new version 2.2.0 that fix the issues with duplicating a graphics directly. The script did not handle the case where a graphic was duplicated directly instead of a folder with a graphic being duplicated.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-02 12:03 AM
That is a typo as the object types are not compatible, even tho it would be nice to have support to convert those objects.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-02 12:37 AM
Version 2.2.1 ?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-02 01:19 AM
It is working now, thank you for your support.
I also tested another scenario where I wanted to replace the Description, Note 1 and Note 2 properties of an object (test made with Function Block Program). The script executed the replacement in the program, but did not replace the template text in it's properties.
I think that this would also be a nice thing to do.
Otherwise, this is a very powerful script, thank you for it!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-08 01:40 AM
I agree, we use description and note properties to assign positions to otherwise generic components, so this would be very nice addition!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-11 02:01 AM
I just released version 2.3.0 of the script that adds support for renaming properties like Description, Note 1, Note 2, Label Text, Alarm message, Reset messages and source name prefix.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-06 03:52 PM
Is there a video demonstration available?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-07 09:07 AM
would specifically like to see a video demonstration of duplicating components in a graphic.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-08 06:43 AM . Last Modified: 2025-11-08 06:45 AM
Hi @barbizo
There is no video available for this.
The script can duplicate objects or whole structures, including TGML graphics, and rename objects and/or texts inside the TGML. However, it does not duplicate individual components within a graphic.
Did I misunderstand what you were looking for?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-10 08:43 AM
If you have time and resources available to make a video I think that would be helpful! Yes that answers my question.
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-01 01:24 AM
Nice tip! Duplicating and renaming SEAL scripts can get confusing, so this walkthrough really helps. Good reminder to update all the internal references after copying.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-02 06:56 AM
Thank you for adding the properties, it helps us a lot.
I would also suggest to add the alarm's 'Category' and 'Category 2' properties.
It would also help us a lot, because we could generate whole devices using SEAL. In this moment, I need to add the alarm categories manually after executing SEAL Duplicate and Rename.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.