Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84753members
354182posts

NetBotz 5.3.1 Release!

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Rick_O
Lieutenant JG Lieutenant JG
Lieutenant JG

NetBotz 5.3.1 Release!

Hello Everyone,

 

I wanted to take this time to announce that we have released NetBotz v5.3.1. 

 

Netbotz 750/755 v5.3.1 release highlights:

 

1.) Fix for CVE-2021-44228

2.) Ability to add up to 10 SNMP Trap Receivers

3.) Various bug fixes and performance improvements.

 

Also included are the benefits from 5.3.0.

 

1.) Mass Configuration ability from both a config.ini upload to the bot as well as thru DCE (ITE functionality coming very soon)

2.) New wireless firmware (for the NBCWC100U, NBWS100H, and NBWS100T)

3.) Enhanced UI (Quicker navigation  and enhance menu structure based on VOC)

4.) Update underlying OS for enhanced performance as well as many OS fixes

5.) Multiple bug fixes

 

The firmware can be downloaded from here SE.com link to the NetBotz v5.3.1 Firmware Download 

 

The full Release Notes for v5.3.1 can be found here SE.com link to the NetBotz v5.3.1 Release Notes 

 

As always we welcome any and all feedback. If you have issues or need help troubleshooting please don't hesitate to reach out to your local tech support representatives.

 

Thanks,
Rick Ogren

NetBotz Global Product Manager 

Tags (1)
5 Replies 5
masolans
Ensign
Ensign
0 Likes
1
2840

Re: NetBotz 5.3.1 Release!

How can add SNMP Trap Receivers?

Tags (1)
Rick_O
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
2836

Re: NetBotz 5.3.1 Release!

Hi @masolans ,

 

SNMP trap receivers are added in the settings menu

 

Settings -> SNMP -> Trap Receivers

 

You can hit the add button and add up to 10 trap receivers.

 

Hope this helps.

 

Thanks,
Rick Ogren

NetBotz Global Product Manager

Tags (1)
ChrisJJ
Cadet
0 Likes
0
2798

Re: NetBotz 5.3.1 Release!

Hi Does this also resolve CVE-2021-45046

 

as it updates  Log4J to 2.16.0

 

Thanks 

Chris 

Tags (1)
shaw_voel
Crewman
Crewman
0 Likes
1
2427

Re: NetBotz 5.3.1 Release!

Hi Sir,

 

The link is down, do you have other link can download?

Thank you.

Tags (1)
gcastoldi
Cadet
0 Likes
0
2384

Re: NetBotz 5.3.1 Release!

Hi,

 

According to Technical Support NetBotz firmware version 5.3.1 has been removed due to certain issues.

 

The previous firmware version 5.2.4 is the one to use.

 

 

Best,

Gino

 

Tags (1)