Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 01:41 PM . Last Modified: 2024-04-09 04:27 AM
Dear all,
I miss my sensors in the aircondition from RZ-01_IRC-1.
Has somebody an idear.
DCO Version: 7.5.0-42470-8540
DCE Version: 7.2.7.25
Aircondition:
3 x Model: ACRC502
3 x Version in DCE: v3.7.5
All ACRC502 have the same sensors:
| Input State: | Open |
| Output State: | Open |
| Active Power Source: | A |
| Rack Inlet Sensor 1: | 29.8 °C |
| Rack Inlet Sensor 2: | 20.8 °C |
| Rack Inlet Sensor 3: | 20.9 °C |
| Filter Differential Pressure: | 27 Pa |
| Fluid Valve Position: | 35 % |
| Fluid Flow: | 0.29 L/s |
| Entering Fluid Temperature: | 9.1 °C |
| Leaving Fluid Temperature: | 9.3 °C |
The Screen is from DCO in DCE I see all values.
But why do I see only 2 sensors in the DCO. In DCE I have more Sensors?

Best regards
Ralf
(CID:99156024)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 01:41 PM . Last Modified: 2024-04-09 04:27 AM
Hi Ralf,
Can you please be more specific? What version of DCE are you using? What is the exact model device you're looking at? What version of firmware is on the devices (working and not working)? Are the devices that show these values different in any way from the device that does not show the values? If you do an SNMPwalk of each device, do they both show these values in their output? What view are you showing in your screenshot, is this DCO or DCE? If this is DCO, can you see the values you're looking for in DCE?
Steve
(CID:99156026)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 01:42 PM . Last Modified: 2023-10-31 11:21 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.