Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

cross connect in same fobot

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • cross connect in same fobot
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Admiral Cory_McDonald Admiral
129
Jef
Admiral Jef Admiral
111
gsterling
Captain gsterling Captain
72
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
Back to EcoStruxure IT Forum
Start a Topic
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

0 Likes
4
1204
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
Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

cross connect in same fobot

Hi Guys

 

I've created a FOBOT (Let's call it FOBOT A) with "New Port Configurations" to represent different slots in the FOBOT. This FOBOT would represent the end of row distribution frame which connects to the other racks within the row.

 

The back connections to other FOBOTS are complete. So for example FOBOT A now has back connections to FOBOT B and FOBOT C, each in different rack.

 

I am trying to connect two devices to each other end to end. So Device B connects to FOBOT B, which then reaches FOBOT A on a back connect. I can do this for Device C and FOBOT C also. However I am having trouble trying to cross connect on the front of FOBOT A within itself, so that the devices are connected, end to end.

 

Is this possible, or must it be done with different types of objects, or multiple objects? When I use the connect tool it does not appear to let you to connect an object to itself.

 

Thanks

 

 

(CID:123345835)

Labels
  • Labels:
  • Data Center Operation
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

0 Likes
2
1204
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
Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

 

Hi SM

Yes it is possible.  Your final step is to use the Connection Tool to make a connection from your FOBOT A to FOBOT A.   In my example I have used RJ45.  PPB has ports 1-5 back to back to PPA 1-5 and PPB 6-10 back to back to PPC 6-10.  

PPB port 1 connects to PPB port 6

 

Cheers

Ed

(CID:123345982)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

In response to DCIM_Support
0 Likes
0
1204
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
Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

Hi Ed

 

Thanks for the reply. I've setup a similar scenario as you've discussed to demonstrate what I'm running into.

PPA

PPB

PPC

 

PPB:1 back connect to PPA:1

PPB13: back connect to PPC:1

 

I can connect the top device to the PPA:1 front and it maps automatically to PPB:1 via I assume the back connect, but I cannot proceed further to do a cross connect within PPB:1 to PPB:13. When using the connect tool in the rack pane I get a not allowed symbol. Also even typing it out in the device route (2nd screenshot) does not give me the option to go in rack to the same patch panel, even though it lists the other patch panels in the rack. Seems like must be doing something blatantly wrong, but don't know what.

 

 

Running version 7.4.5, using the patch panels in the pre-existing Genomes.

 

Thanks

SM

 

(CID:123346383)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

In response to DCIM_Support
0 Likes
0
1204
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
Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2024-04-07 11:44 PM

Ah ha, I suspect your old DCO version is what's causing you the issue - my test was 8.x  You might confirm my guess by trawling the release notes or contacting SE support (or perhaps someone else might post and confirm)

Cheers

(CID:123346396)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2023-10-22 04:28 AM

0 Likes
0
1204
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
Posted: ‎2020-07-03 06:46 PM . Last Modified: ‎2023-10-22 04:28 AM

superhero.png

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.