If my repository is full and I add another repository will it automatically start to add data in the new repository

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • If my repository is full and I add another repository will it automatically start to add data in the new repository
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Admiral Cory_McDonald Admiral
128
Jef
Admiral Jef Admiral
111
gsterling
Captain gsterling Captain
72
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
Solved Go to Solution
Back to EcoStruxure IT Forum
Start a Topic
Solved
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

0 Likes
2
711
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
Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

If my repository is full and I add another repository will it automatically start to add data in the new repository

(CID:106203634)

Labels
  • Labels:
  • Data Center Expert
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

0 Likes
0
711
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
Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

Hi Luke,

 

I'm going to first assume that the current repository is the local repository. If you add another repository, DCE will start using it based on it's settings. You can add a repository but the system itself will determine when it is time to use the remote repository.  You can also set it to "Use Remote Storage Only" in which case it should start using the remote immediately. You can also migrate the data to the remote repository.

If on the other hand you have a local repository and also have a current remote but are adding yet another remote, there is no way to command the system to use one remote over the other. You can still command it to use remote only but you can not specify which. The system will also send the data to whichever repository it deems correct. I have no algorithm for this.

 

In either case, you can add a remote repository and the system will use it.

 

Steve 

(CID:106203694)

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

0 Likes
0
712
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
Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2024-04-09 12:13 AM

Hi Luke,

 

I'm going to first assume that the current repository is the local repository. If you add another repository, DCE will start using it based on it's settings. You can add a repository but the system itself will determine when it is time to use the remote repository.  You can also set it to "Use Remote Storage Only" in which case it should start using the remote immediately. You can also migrate the data to the remote repository.

If on the other hand you have a local repository and also have a current remote but are adding yet another remote, there is no way to command the system to use one remote over the other. You can still command it to use remote only but you can not specify which. The system will also send the data to whichever repository it deems correct. I have no algorithm for this.

 

In either case, you can add a remote repository and the system will use it.

 

Steve 

(CID:106203694)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2023-10-31 11:08 PM

0 Likes
0
711
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
Posted: ‎2020-07-03 02:39 AM . Last Modified: ‎2023-10-31 11:08 PM

superhero.png

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.