Ask our Experts
Didn't find what you are looking for? Ask our experts!
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
Dear Support team ,
Greetings! We have issue here on one of the site where the sales team has shared the solution with the below DCO server to customer & now we cannot configure our DCO on this server. It is not supporting our Operating system.
Pls advise?
Meanwhile, we have requested the customer to replace the server with RED hatt. server with the config matching our DCO, but he needs an confirmation email on the subject.
Server details.
CPU: 8 cores
Memory: 16 GB RAM
100 GB storage, speed minimum 170 MB/s
Provide any machine which complies with these specs. If your presales team confirms that the below SKUs comply with the aforementioned requirements, please to provide the same to IBM asap and lets close the subject matter;
SKU Description Q-ty
SR730-E5-2630V3
Rail & cable PowerEdge R730 :Intel Xeon E5-2630v3 2.4GHz,20MCache,8.00GT/s QPI,Turbo,HT,8C/16T(85W) Max Mem 1866MHz,2X 8 GBRDIMM, 2133 MT/s, Dual Rank, x4 Data Width,VFlash, 8 GB SD Card for iDRAC Enterprise,PERC H730Integrated RAID Controller, 1GBCache, No Hard Drive, Dual, Hot-plug, Redundant Power,3Yr -NBD. 1
370-ABUN 8GB RDIMM,2133MT/s, DualRank. 1
400-AEEK 300GB 15KRPM SAS 6Gbps 2.5in Hot-plug Hard Drive,3.5in HYB CARR,13G,CusKit 1
(CID:105465964)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
The system requirements depend on the size of the solution, see System Requirements for details.
The Debian version of DCO 7.5 is a .iso file, complete with operating system and all, that you will install on the system.
The Red Hat version is an application package (.rpm file) for Red Hat Enterprise Linux 6.
(CID:105465973)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
Thanks for the email. The issue here is when our FSR try to install the DCO with the server supplied, it doesn't detect the hardware. All the methadology is applied but its No success. It doesnot supportin linux 6. Pls advise solution or do we have to recommend them to order new server Red hat which supports linux 6.
Thanks to respond
Yasser
Schneider Electric
(CID:105465999)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
I'm not sure I understand if you are trying to install the ISO (with Debian)? If that's the case, then you may try installing using alternative drivers which support newer hardware. See http://dcimsupport.apc.com/display/UAOp74/Installing+StruxureWare+Data+Center+Operation#InstallingSt...
(CID:105466000)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
After many attempts to install DCO system using USB bootable image and DVD, with no luck because of system miss compatibility with the server hardware. So after our discussions as per your request to move to installing DCO system on ESXi hypervisor and install DCO system on Virtual Machine to avoid the hardware miss compatibility in order to complete the DCO installation. The installation has been successful with the following below: - ESXi 6 u1 installed as a hypervisor on the server with IP address x.x.x.201 o Esxi username: root o Esxi password: xxxx - DCO has been installed on ESXi with IP address x.x.x.205 o DCO username: apc o DCO password: xxx The user will connect to DCO system from web interface with IP address x.x.x.205 as per attached file. Note: ESXi 6 is on trial version which is valid only for 60 days. Prior to this period ends you need get the required license. .
(CID:105466003)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:57 PM . Last Modified: 2024-04-09 01:03 AM
The license has expired and now the server supplier s charging usfor the license. Pls advise?
(CID:105466004)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:58 PM . Last Modified: 2024-04-09 01:03 AM
Hi Mohammad, You can follow this guide on how to get and install a free license for ESXi 6. http://www.vmwarearena.com/vsphere-6-0-download-free-esxi-6-0-license-keys/
(CID:105466005)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:58 PM . Last Modified: 2023-10-31 10:52 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.