Ask our Experts
Didn't find what you are looking for? Ask our experts!
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:37 AM . Last Modified: 2024-04-10 12:49 AM
Hello,
I want to create a network connection between 2 cabinets which are located in 2 different rooms in the same building. Is this possible? How can I create that connection?
Thanks,
(CID:93915269)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:37 AM . Last Modified: 2024-04-10 12:49 AM
Hi Kaan,
This is possible by interconnecting the patch-panels in the cabinets you need to be networked together.
Here is a way to achieve this:
a. Right click on the patch panel & go to properties.
b. Under "Back Connections" sector, press the button "Connect To"
c. You shall be able to select the exact Room, Row, Rack, Patch Panel, Name, Type & Start Port from there.
I hope this helps.
(CID:93915346)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:37 AM . Last Modified: 2024-04-10 12:49 AM
Hi Kaan, Further to the above answer it is also possible to create a route directly from a device in one cabinet in a room to a device in a cabinet based in another room. This can be done be using the "-> - outside of rack" option which then will present other rooms in the solution. However make sure the room(s) you want to connect to are open in the client since they need to be loaded in order to be presented in the list of available connection.
(CID:93915386)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:37 AM . Last Modified: 2023-10-31 10:50 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.