Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 05:22 PM . Last Modified: 2024-04-03 03:23 AM
Hi
As you can see in the picture below, i configured IP for port number 2 - 10.0.0.1.
At the other edge of this port there is a server, but if i configure its IP address i can configure totally different IP while it should be exactly the same...
How come it is happening ? Why isn't there some process that blocks me from doing that, just like port number 1 in this example (of course IP address of 65000 is invalid so the system gives me an alarm "Invalid format").
Of course i won't do this on purpose but if it happens in a mistake it might does collisions in the system...
Thanks,
Sheep 😀
(CID:140219608)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 05:22 PM . Last Modified: 2024-04-03 03:23 AM
Hello Sheep.
DCO does not currently have the context regarding what is actually present on a network connection so it may not be fair to assume the data on both ends of the connection has to be the same. Although perhaps there's a feature request here which allows the customer to enable this check?
For example the connection from one port to another could be a trunk connection on which many IP's are present or I have heard some customers who use connections from a server to their DMZ to record the server IP on the server side, the DMZ/internet facing IP on the DMZ connection side.
Regards
Greg Sterling
(CID:140711805)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 05:22 PM . Last Modified: 2023-10-22 01:38 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.