Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DCE active alarms delay

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • DCE active alarms delay
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
mosheshiper
mosheshiper
Contributor

Posted: ‎2022-06-15 08:49 PM

0 Likes
1
1081
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
Posted: ‎2022-06-15 08:49 PM

DCE active alarms delay

Hello

I have dce 7.7.1 and I have delay on active alarms.

I configured threshold alarm for max temperature 26 degrees on my pdu sensor as critical.

 I use Apc pdu.

When the temperature increase above 26 degrease I suppose to get red critical alarm at the

Active alarms section. Most of the times it take 15 minutes to show up and not immediately.

So happened when the temp return to normal. The global scan interval is 1 minutes. Its not

A server problem because the cpu and memory not loaded (50%). Its happened also

With current and other thresholds I have and for all sensors. When I mark the alarm

generation in the PDU to enable , the device  Alarm show immediately at the active alarms.

 I check everything and have no idea Why it happened

Thanks

Labels
  • Labels:
  • Data Center Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2024-05-03 05:25 AM . Last Modified: ‎2024-05-03 05:26 AM

1 Like
0
730
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
Posted: ‎2024-05-03 05:25 AM . Last Modified: ‎2024-05-03 05:26 AM

Hi @mosheshiper,

 

I know it has been some time since this post was created, but wanted to get a response out there in case other came across a similar issue.

From my experience I do not recommend a global scanning internal of 1 minute.  For APC devices I recommend using priority scanning, which is a method where the APC device sends a request to DCE to poll it when an alarm goes active on the end-device.  If the alarm is active at the time the polling occurs, then DCE would get the alarm and do the necessary actions with in.  This option does not exist for 3rd party devices.

 

If it is taking up to 15 minutes to show up in the client, I would lean on it being performance related.  As you have stated your RAM/CPU are okay for overall utilization, but in regards to software performance, it would be wise to investigate using our DCE performance troubleshooting guide: https://community.se.com/t5/Data-Center-Expert-Virtual/DCE-performance-troubleshooting-guide/ta-p/44...

 

I would also suggest reaching out to technical support so that they can investigate the logs as well to see what is going on your server and/or desktop client.

 

Regards,

Cory
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.