Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DCE - UPS - Device Alarm Configuration = missing parameters for Symmetra PX + DDF

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • DCE - UPS - Device Alarm Configuration = missing parameters for Symmetra PX + DDF
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
160
Jef
Jef Leader
114
gsterling
gsterling Mentor
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
Back to EcoStruxure IT Forum
Start a Topic
Solved
SM2
SM2
Explorer

Posted: ‎2024-07-02 10:44 AM

0 Likes
2
1364
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
Posted: ‎2024-07-02 10:44 AM

DCE - UPS - Device Alarm Configuration = missing parameters for Symmetra PX + DDF

Hi 

 

I have DCE 7.8.1. I added a couple symmetra PX 40k UPS recently but in the Device Alarm Configuration , there are a lot of missing alarms that are available in the UPS web interface. I have On Battery Power wherever on Device alarm configuration I don't have it. When there is a power outage I don't have the alarm and to know if we had a power outage I need to look in the UPS log to know if there was a input power problem and if the UPS was on battery. 

 

There is many Device Alarm Configuration but they are not the same as in the web / UPS log. 

 

What is the DDF used for Symmetra PX UPS? 

 

Is it because I don't have an up to date ddf file? What is causing this? PLease help me understand.
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
ATrabert
ATrabert Mentor
Mentor

Posted: ‎2024-09-30 06:21 AM

0 Likes
0
1242
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
Posted: ‎2024-09-30 06:21 AM

Hi,

As long as the Device Alarms page is populated in DCE and you do not have an alarm in DCE about  "Device Status may be inaccurate due to DDF file transfer" https://www.apc.com/us/en/faqs/FA177004/ , then DCE should have all the alarms for the device.  The on battery alarm may be worded a little differently like "loss of input power"

When you discovered the device in DCE, Was priority scanning enabled and are SNMP writes enabled on the device, does DCE have the correct write community string? 
- you can check this in Device->snmp device comm settings ->snmp device scan settings
FAQ what is priority scanning

https://www.apc.com/us/en/faqs/FA271584/

 

How long do your on battery event's last?  Less than a minute? Less than 15 seconds?

-if priority scanning is not enabled, than DCE will use the polling interval of the device, default is 5 mins.  Even with priority scanning, events have to last at least 15-30 seconds so that the device can send DCE a trap and DCE can go poll the device and get any active alarms.  If your load transfers to generator in 10 seconds, then you may never see the on battery event in DCE

 

What is the firmware version on the network card?
 


See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
ATrabert
ATrabert Mentor
Mentor

Posted: ‎2024-09-30 06:21 AM

0 Likes
0
1243
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
Posted: ‎2024-09-30 06:21 AM

Hi,

As long as the Device Alarms page is populated in DCE and you do not have an alarm in DCE about  "Device Status may be inaccurate due to DDF file transfer" https://www.apc.com/us/en/faqs/FA177004/ , then DCE should have all the alarms for the device.  The on battery alarm may be worded a little differently like "loss of input power"

When you discovered the device in DCE, Was priority scanning enabled and are SNMP writes enabled on the device, does DCE have the correct write community string? 
- you can check this in Device->snmp device comm settings ->snmp device scan settings
FAQ what is priority scanning

https://www.apc.com/us/en/faqs/FA271584/

 

How long do your on battery event's last?  Less than a minute? Less than 15 seconds?

-if priority scanning is not enabled, than DCE will use the polling interval of the device, default is 5 mins.  Even with priority scanning, events have to last at least 15-30 seconds so that the device can send DCE a trap and DCE can go poll the device and get any active alarms.  If your load transfers to generator in 10 seconds, then you may never see the on battery event in DCE

 

What is the firmware version on the network card?
 


Reply

Link copied. Please paste this link to share this article on your social media post.

SM2
SM2
Explorer

Posted: ‎2024-10-18 07:01 AM

0 Likes
0
1179
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
Posted: ‎2024-10-18 07:01 AM

Hi! thanks for your input.

 

Priority scanning is active but as you mentioned, events are too short to be registered in DCE. I have activated emails alerts directly on devices as a workaround. I may have around 10+ UPS on different datacenter which exhibit the same behavior so it's not a firmware or a a specific models. (UPS includes Galaxy VM, PW, Symmetra PX etx...)  Some of them I could connect a DryContact on the transfer switch but on a UPS level I won't be able to catch an input transfert otherwise...

 

thank you!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.