Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DCE Modbus "action alarm location problem "

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • DCE Modbus "action alarm location problem "
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
160
Jef
Jef Leader
114
gsterling
gsterling Mentor
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
Back to EcoStruxure IT Forum
Start a Topic
Solved
poomsee
poomsee
Explorer

Posted: ‎2023-02-07 01:29 AM

1 Like
1
1003
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
Posted: ‎2023-02-07 01:29 AM

DCE Modbus "action alarm location problem "

I have add the location option in the "add custom property " section, picture number two, but at the time of the incident, the location and position is empty in the active alarms section. Number one pic

picture 2.pngpicture 1.png

Labels
  • Labels:
  • Data Center Expert
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
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2024-05-06 09:18 PM

1 Like
0
756
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
Posted: ‎2024-05-06 09:18 PM

Hi @poomsee,

 

The column that you added is actually the default Location column that exists within DCE. The location value would be the location pulled from the device identification OID that is set directly on the device itself.

 

The Custom property for location that you created is not able to be added into the the Active Alarms view.  Custom properties can however be added into the Device View.  Views that can have a custom property added would like like this within the Configure Columns view:

Cory_McDonald_0-1715055276110.png

 

Regards,

Cory

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2024-05-06 09:18 PM

1 Like
0
757
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
Posted: ‎2024-05-06 09:18 PM

Hi @poomsee,

 

The column that you added is actually the default Location column that exists within DCE. The location value would be the location pulled from the device identification OID that is set directly on the device itself.

 

The Custom property for location that you created is not able to be added into the the Active Alarms view.  Custom properties can however be added into the Device View.  Views that can have a custom property added would like like this within the Configure Columns view:

Cory_McDonald_0-1715055276110.png

 

Regards,

Cory
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.