Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-05 07:31 AM
Dear Community,
I have received a complaint from our end-user recently:
They are using Aruba access switch and with ClearPass authentication :
The access first detected the mac address is d4:xx:xx:xx:eb:e1 (The MAC address of GB2 is d4:xx:xx:xx:eb:e0) and not the d4:xx:xx:xx:eb:df (MAC address of GB1) that is showed on the DCE.
The first mac address will go to time-out after a day, after that, the DCE IP address will not reachable due to the policy that only authorized MAC address is allowed to connect. After DCE reboots, it happens that the DCE connection shows the first mac address again, which is d4:xx:xx:xx:eb:e1
Does anyone come across this issue before?
BR,
TJ
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-05 08:17 AM
Hi TJ,
Some questions, and an educated guess ..
My speculation is that a management interface is active on Gb1. On larger servers idrac etc have their own ethernet port - but on servers without a dedicated port, they share the first ethernet port. And since the management controller will be raised earlier in the boot than the OS is, this may be the first address their switch is capturing. A packet capture (at the switch) would be very useful in proving what's occurring on this interface before the OS starts using d4:xx:xx:xx:eb:df.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-06 02:16 AM
Hi Shaun,
- This is an old configuration > 5 years
- I will ask users which mac address is answering the IP when they access the system. Also, if they are willing to do a network capture on Gb1 later.
- No separate management interface. It could be using Gb1 as Idrac port as you mentioned.
Let me forward the information to the users. I guess you hit the key point where the IDRAC might be detected during boot up.
Thank you and Best Regards,
TJ.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-08 10:35 PM . Last Modified: 2021-08-09 08:54 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-08 10:35 PM . Last Modified: 2021-08-09 08:54 PM
Hello, @Shaun
As discussed in detail in Chapter 5, “Number Systems,” in networking, IPv4 addresses are represented using the decimal (base 10) number system and the binary (base 2) number system. IPv6 addresses and Ethernet addresses are represented using the hexadecimal (base 16) number system. To understand hexadecimal, you must first be very familiar with binary and decimal.
The hexadecimal numbering system uses the numbers 0 to 9 and the letters A to F.
An Ethernet MAC address consists of a 48-bit binary value. Hexadecimal is used to identify an Ethernet address because a single hexadecimal digit represents 4 binary bits. Therefore, a 48-bit Ethernet MAC address can be expressed using only 12 hexadecimal values.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.