Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Connect to Switched PDU Rack with diff IP address

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Connect to Switched PDU Rack with diff IP address
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
liorf83
liorf83
Explorer

Posted: ‎2024-08-19 05:43 AM

0 Likes
5
1979
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
Posted: ‎2024-08-19 05:43 AM

Connect to Switched PDU Rack with diff IP address

Hi,

I have the following product and I want to connect with several different IP addresses.

There is option to do it?

Attachments
  • Tags:
  • "PDU RACK"
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
dpierce4776
dpierce4776
Troubleshooter

Posted: ‎2024-08-20 06:26 AM

0 Likes
1
1945
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
Posted: ‎2024-08-20 06:26 AM

Sorry but I have a question.

When you say "I want to connect with several different IP addresses. There is option to do it?" Are you saying

 

1. that you want to connect to the PDU FROM several different IP address? Like you have the PDU in one location and people from other locations want to connect to it?

2. Are you saying that you want to the PDU itself to have several different IP addresses?

 

If #1 is true then sure all you need to do is give the PDU an IP address subnet mask and gateway on its local network. From there baring any firewall blocks then anyone can connect to the PDU given that they have the log in information. You can also set different users to different abilitites like administrator that can do anything on the PDU. Device viewers that can see and make some changes. and lastly readonly which can see what the PDU is doing but make no changes.

 

If #2 is correct the answer is no and I ask why you would want to 

Reply

Link copied. Please paste this link to share this article on your social media post.

liorf83
liorf83
Explorer

Posted: ‎2024-08-20 09:32 AM

In response to dpierce4776
0 Likes
0
1903
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
Posted: ‎2024-08-20 09:32 AM

Tnx.1 is correct.i have 8 devices connect to pdu and i want to control on pdu from 8 devices with diff ip adress.can i do it?

Reply

Link copied. Please paste this link to share this article on your social media post.

liorf83
liorf83
Explorer

Posted: ‎2024-08-20 11:30 AM

0 Likes
2
1903
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
Posted: ‎2024-08-20 11:30 AM

The reason that i am is asking is becouse i am trying to reach thd pdu from 2 diff device paralel and somtimes i get pipe broken.where i need to configure the gateway?

Reply

Link copied. Please paste this link to share this article on your social media post.

dpierce4776
dpierce4776
Troubleshooter

Posted: ‎2024-08-22 12:02 PM

In response to liorf83
0 Likes
1
1843
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
Posted: ‎2024-08-22 12:02 PM

The gateway should be set to the devices local LAN gateway. From there unless there is firewall blocks you should be able to reach the PDU from any device. That said sometimes if you have two different connections at the same time both trying to make changes or the like then the system may get hung for a second. 

 

May I ask why you are trying to control or use the web interface of the PDU from 2 locations at the same time?

Reply

Link copied. Please paste this link to share this article on your social media post.

liorf83
liorf83
Explorer

Posted: ‎2024-08-25 01:30 AM

In response to dpierce4776
0 Likes
0
1779
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
Posted: ‎2024-08-25 01:30 AM

i have 2 processes that install on 2 diff devices and they are running parallel and sometimes they are trying to reach the PDU in the same time and i get broken pipe.

Why the solution is configure gateway?  
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.