Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:00 AM . Last Modified: 2024-04-09 12:25 AM
Dear Team,
We just got a confirmation from a Client is Bahrain that they have arranged a Cisco UCS Server for StruxureWare DCE, DCO and Portal deployment with Vmware Set Up with the attached specification.
Can the DCE, DCO and Portal be deployed in the below Server Specs.xlsx :
| Line Number | Part Number | Description |
| 2.0 | UCSC-C220-M4S | UCS C220 M4 SFF w/o CPU, mem, HD, PCIe, PSU, rail kit |
| 2.0.1 | CON-SNT-C220M4S | SNTC-8X5XNBD UCS C220 M4 SFF w/o CPU, mem, HD |
| 2.1 | UCS-CPU-E52630D | 2.40 GHz E5-2630 v3/85W 8C/20MB Cache/DDR4 1866MHz |
| 2.2 | UCS-MR-1X322RU-A | 32GB DDR4-2133-MHz RDIMM/PC4-17000/dual rank/x4/1.2v |
| 2.3 | A03-D300GA2 | 300GB 6Gb SAS 10K RPM SFF HDD/hot plug/drive sled mounted |
| 2.4 | UCS-HD12TB10K12G | 1.2 TB 12G SAS 10K RPM SFF HDD |
| 2.5 | UCSC-PCIE-IRJ45 | Intel i350 Quad Port 1Gb Adapter |
| 2.6 | UCSC-CMAF-M4 | Reversible CMA for C220 M4 friction & ball bearing rail kits |
| 2.7 | UCSC-RAILB-M4 | Ball Bearing Rail Kit for C220 M4 and C240 M4 rack servers |
| 2.8 | UCSC-PSU1-770W | 770W AC Hot-Plug Power Supply for 1U C-Series Rack Server |
| 2.9 | CAB-9K10A-UK | Power Cord, 250VAC 10A BS1363 Plug (13 A fuse), UK |
| 2.1 | N20-BBLKD | UCS 2.5 inch HDD blanking panel |
| 2.11 | UCSC-HS-C220M4 | Heat sink for UCS C220 M4 rack servers |
| 2.12 | UCSC-MLOM-BLK | MLOM Blanking Panel |
| 2.13 | VMW-VSP-STD-3A | VMware vSphere 6 Standard (1 CPU), 3-yr, Support Required |
| 2.13.0.1 | CON-ISV1-VSXSTD3A | VSphere Standard for 1 CPU; ANNUAL List 3-YR Reqd |
| 2.14 | UCSC-MRAID12G | Cisco 12G SAS Modular Raid Controller |
| 2.15 | C1UCS-OPT-OUT | Cisco ONE Data Center Compute Opt Out Option |
(CID:105471106)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:00 AM . Last Modified: 2024-04-09 12:25 AM
Hi Dhiman
It should be possible to run the DCO and DCE on VMware, as long as the minimum requirements are met for each software.
Only concern is that DCO and DCE will share the cores and memory of the one server you listed, so if i.e DCE are using a lot of resources to scan a lot of devices the DCO server might be affected.
Hope that helps
Jesper Thomsen
(CID:105471114)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:00 AM . Last Modified: 2024-04-09 12:25 AM
Hi Dhiman
It should be possible to run the DCO and DCE on VMware, as long as the minimum requirements are met for each software.
Only concern is that DCO and DCE will share the cores and memory of the one server you listed, so if i.e DCE are using a lot of resources to scan a lot of devices the DCO server might be affected.
Hope that helps
Jesper Thomsen
(CID:105471114)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:00 AM . Last Modified: 2024-04-09 12:25 AM
Dear Jesper, Thanks a lot for the prompt response. I will make sure that the Client is aware of the utilization of the CPU with regards to the three applications. As of now there will not be too much of traffic in the DC Expert as the solution is for only 50 Racks with 10 Rack PDUs and 2 UPS. Total nodes will be around 20. Thanking you once again and wishing you a great day ! Regards, Dhiman Das
(CID:105471120)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:00 AM . Last Modified: 2023-10-31 10:19 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.