Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:01 PM . Last Modified: 2024-04-03 12:16 AM
Dear Team,
I have a customer who has RDU -A G2 Environmental monitoring system and Liebert GXT4 3kVA UPS.
I have tried to add the two devices on DCE but DCE can't find them even after specifying the exact IP address using SNMP V1 and V3.
Kindly advise if DCE can monitor these devices.
Thank you.
Regards.
(CID:150732808)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:01 PM . Last Modified: 2024-04-03 12:16 AM
DCE should be able to monitor almost any Liebert/Vertiv device out of the box with the pre-installed Liebert DDF. Did you make sure to whitelist DCE's ip address as a nms in the vertiv/liebert web card? You can find this under communications-->snmp–>snmp v1 access control in the web card. Also make sure you are using the correct community strings.
Another way to test that DCE is able to communicate to the device using snmp properly is do a snmp device walk. In the latest versions of DCE, you can access this tool from the DCE web page–>status and then change the drop down to snmp device walk. You may also want to verify DCE can ping the device, which can also be found on the status page under "troubleshoot network"
(CID:150732826)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:01 PM . Last Modified: 2024-04-03 12:16 AM
DCE should be able to monitor almost any Liebert/Vertiv device out of the box with the pre-installed Liebert DDF. Did you make sure to whitelist DCE's ip address as a nms in the vertiv/liebert web card? You can find this under communications-->snmp–>snmp v1 access control in the web card. Also make sure you are using the correct community strings.
Another way to test that DCE is able to communicate to the device using snmp properly is do a snmp device walk. In the latest versions of DCE, you can access this tool from the DCE web page–>status and then change the drop down to snmp device walk. You may also want to verify DCE can ping the device, which can also be found on the status page under "troubleshoot network"
(CID:150732826)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:02 PM . Last Modified: 2023-10-20 05:04 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.