Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-03-01 10:26 PM . Last Modified: 2023-05-02 11:58 PM
I've been having a play with Geo SCADA performance counters and have successfully gotten them to update the corresponding OPC tags under the PerformanceStats aggregate.
Just wondering what is the recommended way to use these on a multi-server setup (Hot standby w/ Permanent Standby)? So far, I've tried the following:
Also, should the Geo SCADA counters be registered on permanent standby servers? Or is this really only useful for main servers?
Cheers
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-03-02 02:29 PM
I've never actually used the Geo SCADA Expert Performance Counters (although they're quite a recent addition also).
Some of the counters (like Query Performance) would be applicable on Permanent Standby servers, but likely it wouldn't be very exciting, unless you have Performance Servers which have significant load applied to them. But then likely the existing Windows Performance Monitor stuff (CPU usage, Memory, disk queue etc) would be a more generic metric of 'server load', which is probably more important to performance than just the Geo SCADA Expert query loading (and arguably you could refine the Windows Performance Monitor stats to just be specific Geo SCADA Expert processes to get QP load etc).
I think your first option is probably the best way to go if you want a display (or history) of the Main server loading.
This is likely the best path for being able to look at regressions in Test/Dev activity also. If a change is about to be imported, but it shows a significant uptick in Queries / Events etc etc then it could be re-assessed as to whether it provides benefits proportionate to it's "cost" (i.e. if it will double your server loading, but it just provides an animated spinning circle.. maybe not worth it)
If you care about showing individual server loads, then you might need to get tricky and use the OPC driver to retrieve the data from the other servers and log to OPC points.
I can't see much use for displaying just the current server stats. It would only be if you had a number of servers clients connected to, and you wanted an easy way for them to report the loading on the server they are connected to if they are complaining about bad performance. But again, it would likely be better to refer to Windows Performance Monitor data then... since it's a better metric of overall server performance.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-03-02 02:29 PM
I've never actually used the Geo SCADA Expert Performance Counters (although they're quite a recent addition also).
Some of the counters (like Query Performance) would be applicable on Permanent Standby servers, but likely it wouldn't be very exciting, unless you have Performance Servers which have significant load applied to them. But then likely the existing Windows Performance Monitor stuff (CPU usage, Memory, disk queue etc) would be a more generic metric of 'server load', which is probably more important to performance than just the Geo SCADA Expert query loading (and arguably you could refine the Windows Performance Monitor stats to just be specific Geo SCADA Expert processes to get QP load etc).
I think your first option is probably the best way to go if you want a display (or history) of the Main server loading.
This is likely the best path for being able to look at regressions in Test/Dev activity also. If a change is about to be imported, but it shows a significant uptick in Queries / Events etc etc then it could be re-assessed as to whether it provides benefits proportionate to it's "cost" (i.e. if it will double your server loading, but it just provides an animated spinning circle.. maybe not worth it)
If you care about showing individual server loads, then you might need to get tricky and use the OPC driver to retrieve the data from the other servers and log to OPC points.
I can't see much use for displaying just the current server stats. It would only be if you had a number of servers clients connected to, and you wanted an easy way for them to report the loading on the server they are connected to if they are complaining about bad performance. But again, it would likely be better to refer to Windows Performance Monitor data then... since it's a better metric of overall server performance.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-04-06 11:26 PM
Thanks, I've had them running for a month now on all our primary/standby servers with no issues and getting some good diagnostic data on main server performance. Can definitely say they are quite handy.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.