Data Center Expert release notes
Contact Support
Submit a support request for additional assistance with EcoStruxure IT software.
Link copied. Please paste this link to share this article on your social media post.
See the list of the server appliances (AP9465, AP9470, and AP9475) supported by DCE 7.9.x and newer:
See Data Center Expert 7.9.x and newer - server hardware requirements
The Data Center Expert desktop client is a stand-alone Java application that runs on systems that meet the following requirements:
Note: See Known Issues in DCE for details about support for Internet Explorer and Edge.
The Data Center Expert 8.2.0 release introduces support for Federal Information Processing Standards (FIPS) for computer systems used by United States government agencies and their contractors.
The cryptographic modules utilized by Data Center Expert are undergoing FIPS 140-3 validation and are currently awaiting CVMP review on the Module in Process List.
The Data Center Expert 8.2.0 release contains improvements including:
The Device > SNMP Device Communication > Device Scan Settings option now includes a setting to change the communication protocol between the device and DCE from SNMPv1 to SNMPv3.
Note: You must also change the communication protocol on the device.
A new column in the Active Alarms and Alarm History views displays the number of comments on each alarm.
A new copy button makes it easier to capture the build information, MAC address, and server serial number from the Help > About display.
The link to the EcoStruxure IT Help Center in the Help menu is now correct.
You can now install the DCE server and/or the DCE desktop client in FIPS mode.
IMPORTANT: FIPS mode requires that certificates must include the Subject Alternative Name with the fully qualified domain name (FQDN) and IP address of the monitored device or connected server. New certificates may be required.
In the device discovery wizard, the Run discovery now option is now checked by default.
When TCP is selected, there is now an option to specify a line terminator, \r\n by default.
The /v1/devices/sensors endpoint was added to the DCE REST API for bulk retrieval of sensors across all devices a caller has access to.
The event log now includes:
Visit the EcoStruxure IT Help Center for more information.
Server operating system
Server OS: Proprietary Rocky Linux 8.10 (RHEL derivative)
Java version: OpenJDK-headless-11.0.24.0.8-3.el8
Windows desktop client
Java version: Adoptium 8u422-b05
Software vulnerabilities fixed in DCE 8.2.0
The security vulnerabilities addressed in this release include:
The following third-party components were updated to address these specific cybersecurity vulnerabilities:
Apache
Linux kernel
This release also includes various additional component updates to improve overall security.
See the Data Center Expert Security section in the Help Center for more information.
The following issues were fixed in DCE 8.2.0:
How to import the APC device firmware update catalog
Complete list of known issues in DCE
The following steps are necessary to update DCE 8.1.0 or 8.1.1 to DCE 8.2.0.
DCE must be at a minimum of 8.1.0 or 8.1.1 to update to DCE 8.2.0. If you are downloading DCE 8.2.0, you will need access to the Internet.
You must have a valid software support contract to receive the DCE 8.2.0 update. If you do not, then you will need to purchase one to receive the update.
The DCE software update files are available in the EcoStruxure IT Entitlements portal.Log in and then click Software Updates. More information...
If the DCE update files are not available in EcoStruxure IT Entitlements, contact your local technical support to verify your support contract and get access to the update file(s) you need.
IMPORTANT: Do not reboot the server during the update.
The DCE 8.2.0 update performs a data migration that takes under an hour for most systems. The data migration can take longer if the system has thousands of devices and years of history, and varies based on several factors:
Number of devices
Number of sensors connected to those devices
Polling interval
Frequency at which sensor values change. For example, input voltage to UPSs can fluctuate throughout the day vs. temperature sensors in a strictly controlled environment that almost always report the same value.
You can see the status of the update on the Data Center Expert web client Home page.
NOTICE: Before beginning an update, remember to run a full backup on your DCE by going to System > Server Administration Settings > Server Backup/Restore, create a backup entry and then click Start.
It is recommended that you perform the server update when you upload the upgrade file to your DCE server. The update will be performed automatically if the server reboots after the upgrade file is uploaded.
Warning: Only perform the steps in this section if directed to do so by a Technical Support technician.
Before You Restore: A system restore will erase all data and restore the DCE hardware server to its factory default settings. Make sure you have a copy of all installed license keys and network settings prior to restore.
Download the restore.iso file to create a bootable USB key, or contact Technical Support for assistance.
For a USB Key, follow the instructions provided in Creating a bootable USB key (Windows or Linux machine).
Place the USB key in the USB port of your DCE appliance.
Reboot DCE.
When the appliance restarts the system restore process begins automatically. This process takes approximately 10 minutes for the 1U DCE Basic, 15 minutes for 1U DCE Standard or 25 minutes for 2U DCE Enterprise.
When the restore is complete, you will be prompted to remove the USB key and hit enter to reboot the server.
Note: If the system boots into the existing DCE version, reboot the server and access the BIOS settings. Adjust the boot sequence to boot from USB first.
Once DCE has restarted, configure the DCE network settings.
Before You Migrate: To migrate a DCE hardware server to a virtual appliance, you must purchase and apply an activation key. Additionally, you must contact APC Support for new node license keys and application license keys for the virtual appliance.
Perform a back up of the DCE hardware server, using the Server Backup/Restore option, accessed from the Server Administration Settings option in the System menu.
Deploy the demo version OVA, and configure it using the hardware equivalents for the DCE Basic, Standard, or Enterprise server from which you are migrating. The available disk space for the virtual appliance must be greater than the disk space used by the hardware server. You cannot restore to a virtual appliance with fewer CPU, fewer network adapters, less RAM, or less available disk space than the hardware server. See help for Deploying and configuring a DCE virtual appliance, and DCE virtual appliance equivalent configurations.
Perform a restore on the virtual appliance, using the Server Backup/Restore option, accessed from the Server Administration Settings option in the System menu. You cannot restore to a virtual machine other than the DCE virtual appliance.
Apply the activation key to the virtual appliance.
Log in to the DCE client. In the "License Keys" display, accessed from the Server Administration Settings option in the System menu, apply the new node license keys and application license keys you received from APC Support.
Instructions for a Windows machine
Insert a 4GB (or larger) USB key into your system.
Extract the following file to a temporary directory:
DCExpertUsbFlashRestore_Win_8.1.1_b.zip
Open a command prompt to the temporary directory and run mkDCExpertRestoreUsbKey.bat <iso image filename>. For example: mkDCExpertRestoreUsbKey.bat c:\tmp\restore.iso
Answer the prompts as appropriate.
Instructions for a Linux machine
Insert a 4GB (or larger) USB key into your system.
Extract the following file to a temporary directory:
DCExpertUsbFlashRestore_Linux_8.1.1_b.tar.gz
Open a command prompt to the temporary directory and run mkDCExpertRestoreUsbKey.sh <iso image filename>. For example: mkDCExpertRestoreUsbKey.sh /tmp/restore.iso
Answer the prompts as appropriate.
Third-party USB key scripts
The scripts used to create USB keys use the following software:
Software |
URL |
Windows |
Linux |
Syslinux |
X |
X |
|
7-zip |
X |
|
|
GNU sed |
X |
|
Link copied. Please paste this link to share this article on your social media post.
There should be an option to download the release notes as a PDF.
Hi @jmcnutt,
Thanks for your feedback.
You can click the Options icon (three dots) and choose Printer friendly page to save an article as a PDF.
May I ask why you find a PDF document useful?
Best,
Jackie
Hi @JLehr
The "printer friendly page" only reformats the page, rather than displaying any kind of download link. I would still be relying on the "print to PDF" function to put together a legible document, which also wouldn't have any kind of table of contents or internal linking. (It would also have these comments at the bottom, which would be weird.)
Any time we install updates on a system - a firewall, for example - the new software/firmware/code is copied to our internal infrastructure file server along with the relevant release notes, in case they are needed for later reference, or by another network admin. Having the release notes as a PDF (as most vendors do) makes this process very easy and also ensures that when I open the release notes, I see the same thing as when my colleagues open them.
Thanks for this @jmcnutt. We're exploring ways to improve this experience.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.