XBK Analyzer tool warning regarding *** possible configuration issue *** (QC#49504)

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • XBK Analyzer tool warning regarding *** possible configuration issue *** (QC#49504)
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
2555 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

XBK Analyzer tool warning regarding *** possible configuration issue *** (QC#49504)

Guinan RobertAndriolo Guinan
‎2024-07-30 12:10 AM

Issue

When using the SBO xbk Analyzer, a warning with the following details is observed: 

  • *** possible configuration issue *** (QC#49504) 
  • Issue: 'Communication failed' alarms between servers, even if no bindings are made
  • Action: Make sure servers can communicate with each other so they can synchronize.

Product Line

EcoStruxure Building Operation

Environment

Building Operation Server backups version 3.x and above. 

Cause

The defect mentioned in the tool (QC#49504 / DBSQA-57599) was initially created because alarms were generated between two (or more) Automation Servers that had no bindings (or references) between them. This behavior is considered normal.


This occurs because the servers attempt to synchronize references but fail due to communication issues, resulting in the alarms. These Automation Servers were previously part of the same system but were separated before reference synchronization was completed.


A possible scenario for this issue is:

  • Two servers can see each other.
  • Bindings are established between the two servers.
  • The connection between the two servers is then disrupted (i.e., offline).
  • Subsequently, one or more of the bindings are deleted, leading to offline alarms between these servers, even if no binding exists now, due to pending synchronization.

Resolution 

The XBK analyzer tool detects this situation via a "SyncPending" flag, indicating that it needs to be investigated if a "Communication Alarm" exists between these servers.


This warning can be ignored if no communication alarms are associated with the servers listed by the analyzer tool.

 

In most cases, if the server names listed by the tool are part of the system, the issue can be resolved by checking and verifying for unresolved bindings via Binding Diagnostics. while connected to a working EBO System.

 

If the tool lists any other server names that are not part of the system, these server names can be cleared by upgrading to EBO 2024 (v6.0.x) and above.  As stated, it is only a warning for earlier versions and can be ignored, as there can be instances where this is not cleared until upgraded to this release.  

 

 

 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (1)
  • Find more articles tagged with:
  • RobertAndriolo24
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.

You’ve reached the end of your document

WHAT’S NEXT?

Ask our Experts

Didn't find what you are looking for? Ask our experts!

My Dashboard

Check out the new Feeds and activities that are relevant to you.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.