Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

When starting OPRIF, the Auto Answer feature is enabled automatically and begins synchronizing with the external modem

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • When starting OPRIF, the Auto Answer feature is enabled automatically and begins synchronizing with the external modem
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Leo_Tantalo
    Leo_Tantalo
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2165 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

When starting OPRIF, the Auto Answer feature is enabled automatically and begins synchronizing with the external modem

Picard Product_Support
‎2018-09-11 02:54 PM

Issue

Trying to use OPRIF to make a few programming changes to a MicroSmart controller. OPRIF is installed on a SIGNAL computer (Windows 98). With SIGNAL disabled, OPRIF is able to start and handshake with the COM port. However the Auto Answer feature is enabled by default and begins an endless loop of trying to synchronize with the modem. The looping effect prevents a proper connection to the DMS to do programming changes. How can the Auto Answer be disabled on startup of OPRIF?

Product Line

TAC IA Series

Environment

OPRIF or Operator Interface version 11.4 and higher

Cause

Initialization file was modified by default

Resolution

The readme.txt file in the DMS folder explains how to prevent Auto Answer from being enabled on startup of OPRIF. Click here to view the entire readme file. Below is the excerpt on how to disable Auto Answer:

Changes to the command strings used for modem-initialization and control

The default modem init-string "AT C1 E1 V1 S0=1 S7=51" has been changed. It is now "AT&C1&D2E1V1".

If you or your modem don't like this string, you can now override the default. Using NOTEPAD or EDIT, create a file called MODEM.INI in the DMS directory. This file should contain a single line of ASCII, which will be your customized initialization string.

The line must begin with the letters "AT", and must not contain the letters "DT". Other than this one restriction, your modem-init string can contain whatever commands your modem requires.

Two separate default strings have been defined for turning auto-answer ON and OFF. These may be overridden by creating files with the appropriate names in the DMS directory.

To specify a customized string to force your modem to STOP auto-answering, use NOTEPAD or EDIT to create file a called ANSWEROF.INI in the DMS directory. By default, this file would contain the single ASCII line "ATS0=0".

If your modem requires a disconnect command, you could instead write a line that reads "ATH ATS0=0".

The default autoanswer ON string "ATS0=1", instructs the modem to answer on the first ring. To answer on the third ring, use NOTEPAD or EDIT to create a file called ANSWERON.INI in the DMS directory. It should contain the single
ASCII line "ATS0=3".

SUMMARY:

Description Default String Filename Comment
Modem Initialize AT&C1&D2E1V1 \DMS\MODEM.INI Modified in 11.4
Auto-answer On ATS0=1 \DMS\ANSWERON.INI New in 11.4
Auto-answer Off ATS0=0 \DMS\ANSWEROF.INI New in 11.4
Labels (1)
Labels:
  • TAC IA Series
Attachments
Tags (1)
  • Find more articles tagged with:
  • 16685
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.