Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

What is the compatibility between various versions of the I/A Series G3 software?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What is the compatibility between various versions of the I/A Series G3 software?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa116868
    sesa116868
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1419 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What is the compatibility between various versions of the I/A Series G3 software?

Picard Product_Support
‎2018-09-06 09:57 AM

Issue

For example:

>  Can a I/A Series G3 3.5.34 station in an ENC be edited with a 3.7.106 release of Workbench?

>  Can a I/A Series G3 3.6.47 station in an ENC be edited with a 3.6.406 release of Workbench?

Environment

I/A Series G3 ENC or JACE controller (any 3.x release)

I/A Series G3 Enterprise Server or Workbench software at any 3.x release

Cause

When engineering a mixed system it is advised that you use the correct version and brand of Workbench to connect. This insures that the modules on your Workbench will be compatible with the modules used by your station.  It is known that connecting with a different set of modules, i.e., different release, can result in a few odd behaviors or display problems or it may not allow you to connect at all.

The incentive to upgrade is primarily for the new features. But it is also convenient to have all your stations at the same build so that you do not have to load different builds of Workbench to properly design and maintain the site.

Resolution

There are two solutions to this issue.

  1. Upgrade the older stations to the latest release.
  2. Install multiple copies of the I/A Series G3 software on the engineering computer and use the appropriate version when editing an existing ENC or JACE station. 

When more than one version of the I/A Series G3 software is installed on the same computer, you must load the corresponding version of the Niagara platform daemon before attempting to use the Workbench software.  There are two ways to load the Niagara platform daemon. 

When newer versions of the I/A Series G3 software are installed, a Windows Start menu folder is created for that version.  The "Install Platform Daemon" command will be found under that folder.  After running that command and allowing the Niagara Daemon service to start, you can use the "Enterprise Network Server" in the same Start menu folder to launch the corresponding release of the Workbench. 

With any version of the I/A Series G3 software, you can manually install & start the platform daemon then start Workbench.  To set the version, start the Niagara console (<release directory>\bin\console.exe) for the version you want to run and then type the command "plat installdaemon".  You can then also start the workbench from that console window by typing "wb" at the command prompt.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 14716
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.