What are the System Requirements for installing MSDE or MSSQL server with a Niagara R2 Enterprise Server?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What are the System Requirements for installing MSDE or MSSQL server with a Niagara R2 Enterprise Server?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Product_Support
    Product_Support
  • sesa119747
    sesa119747
  • DavidFisher
    DavidFisher

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1592 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What are the System Requirements for installing MSDE or MSSQL server with a Niagara R2 Enterprise Server?

Picard Product_Support
‎2018-09-07 02:12 AM

Issue

What are the System Requirements for installing MSDE or MSSQL server with a Niagara R2 Enterprise Server?

Environment

  • Niagara R2 Enterprise Server
  • MSDE or MSSQL server

Cause

Hardware and Operating System (OS) must meet the minimum requirements to run MSDE or MSSQL server.

Resolution

These are the following minimum hardware and operating system requirements (per Microsoft’s web site) to run the MSDE database:

• Pentium III, 500-MHz or higher processor.
• Minimum of 512 MB of RAM, 1 GB recommended.
• Minimum of 1 GB of available hard disk space, 3 GB for applications that need more archiving capacity.

The following operating system configurations can run the MSDE:
• Windows XP Professional
• Windows NT Workstation 4.0 with Service Pack 5 or later Supported Software
Supported Database Implementations
• Windows NT Server 4.0 with Service Pack 5 or later
• Windows NT version 4.0 Server Enterprise Edition with Service Pack 5 or later
• Windows 2000 Professional
• Windows 2000 Server
• Windows 2000 Advanced Server
Microsoft asserts that the SQL Server 2000 Driver for JDBC (required for MSDE) has been tested and certified on the following operating systems:
• Microsoft Windows XP
• Microsoft Windows 2000 with Service Pack 2 or higher

The following versions of the JDK are supported for use with the SQL Server 2000 Driver for JDBC:
• JDK 1.1.8
• JDK 1.2
• JDK 1.3
The Microsoft SQL Server 2000 Driver for JDBC is available for download from microsoft.com to all licensed SQL Server 2000 customers at no charge. Review the end-user license agreement (included with the download) for further details on users’ rights.

Note:  A MSDE database can run on a machine other than the Enterprise Server and have the server station write data to the database. For information on the system requirements for a remote MSDE installation, visit http://msdn.microsoft.com/library. This configuration is not supported by Schneider-Electric. 

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 2702
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.