Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Upgrading Smartphone/PDA to Mobile 6 for use with Roam I/O 2 (Revised 3/26/08)

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Upgrading Smartphone/PDA to Mobile 6 for use with Roam I/O 2 (Revised 3/26/08)
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa119747
    sesa119747
  • Carl_Slack
    Carl_Slack
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1260 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Upgrading Smartphone/PDA to Mobile 6 for use with Roam I/O 2 (Revised 3/26/08)

Picard Product_Support
‎2018-09-06 02:49 PM

Issue

Upgrading Smartphone/PDA to Mobile 6 for use with Roam I/O 2

Environment

  • Smartphone
  • Handheld PDA (Personal Digital Assistant)
  • Roam I/O 2 software

Cause

Upgrade existing Smartphone/PDA to Windows Mobile 6 Professional.

Resolution

If upgrading a Smartphone or PDA device to Microsoft's Mobile 6 from a device that was previously used to install the Roam I/O 2 software on to the Smartphone or PDA you'll need to remove the BacnetServiceToolPPC and the InfinetServiceToolPPCusing using the add or remove programs located in the PC's control panel. If you are installing the Roam I/O 2 software from a machine that has not previously had the BacnetServiceToolPPC or InfinetServiceToolPPC installed then there is no need to remove.

Since Mobile 6 was not available when this tool was released, the Roam I/O 2 Pocket PC Requirements do not list that Mobile 6 is supported along with Active Sync 4.5 which is required to synchronize with Mobile 6. We've run some preliminary tests on this platform and find that the functionality remains the same as earlier supported versions of Microsoft's Mobile 2003 & 5.0 which were tested before releasing the Roam I/O 2.

*****************NOTE***********************
There are two different versions of Windows Mobile 6
Windows Mobile 6 Professional --- WILL WORK
Windows Mobile 6 Standard --- WILL NOT WORK

The big difference is that the standard version doe not have touch screen ability which is required with the Roam IO/2 software.

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 2977
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.