Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Third Party ASCII integration

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Third Party ASCII integration
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Product_Support
    Product_Support
  • PaulFr
    PaulFr
  • sesa119747
    sesa119747

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2121 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Third Party ASCII integration

Picard Product_Support
‎2018-09-11 01:40 AM

Issue

Do I need an X Driver to send simple ASCII strings to a third party system?

Environment

Plain English Drivers

PE Driver, Raw Mode

CX Controllers

Netcontroller II

bCX

ACX

Cause

Require the limitations of Plain English drivers

Resolution

It is possible to create a Plain English driver to print ASCII data out of a Comm port.

Use the Open, Close and Print keywords to develop your program in a CX or bCX controller, if you go to the "Help, Contents" on Cyberstation Explorer you can enter these keywords and get full details on their use including example programs. You can also read responses from the 3rd party system with the "Read" keyword.

The Plain English program would be able to print out any information that can be put into an InfinityString. The characters that a PE Driver cannot handle are the FFh (255) and 0H (null) characters, to use these would require the use of an X Driver or another form of gateway to an open protocol.

If you have a first generation controller (CX9900, CX9400 etc) there is a Generic ASCII "X Driver Filter" that can be used to print/ read an ASCII string with no character limitations. If the port is X Driver enabled then download software X-Driver Filter

The CHR keyword can be used to send "Non printable characters".

The other thing is that a Plain English Driver will be dependent on the controller scan time so it would not be suitable for any protocols that are timing critical and the controller scan time must be kept low.

As a general rule of thumb, if you can send the required characters out using Hyperterminal and the system accepts it, then a PE program should be able to send them too. 

The attached document is an example of a Plain English driver that was written a while ago to communicate with a Video Recorder over an RS232 link, the principles and techniques used in this example show the use of the above keywords as well as some of the string manipulation keywords. Download it here.

This also applies to the ACX57xx controllers but they only have a single half duplex RS485 port which may not be suitable for all applications.

Labels (1)
Labels:
  • Andover Continuum
Attachments
ExampleCXDriver.zip
Tags (1)
  • Find more articles tagged with:
  • 11561
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.