Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

The Niagara G3 platform daemon will not run using an administrator account in Windows.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • The Niagara G3 platform daemon will not run using an administrator account in Windows.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • sesa119747
    sesa119747
  • sesa116871
    sesa116871
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4991 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

The Niagara G3 platform daemon will not run using an administrator account in Windows.

Picard Product_Support
‎2018-09-06 02:55 PM

Issue

The Niagara G3 platform daemon will not run using an administrator account in Windows.

Product Line

TAC IA Series

Environment

Niagara G3

Cause

Possible causes:

  1. The niagara service is not started
  2. IIS is running on the computer
  3. Port 3011 is blocked
  4. Authentication

Resolution

There are a number of possible causes:

  1. The niagara service is not started. Run Platform Daemon (Start > Programs > Vykon AX Supervisor > Install Platform Daemon)
  2. IIS is running on the computer.  Disable IIS in Control Panel > Administrative Tools > Services
  3. Port 3011 is blocked. Ensure there are no firewall, antivirus, or remote access software blocking port 3011
  4. There are two types of platform authentication:
    1. Basic platform authentication (the default for a Windows-based host) provides integration with existing Windows installations, and provides two levels of platform access, which are determined by a user’s group membership(s). The levels of platform access are:
      • User - Platform access at this level allows full use of most Workbench platform views. This includes the ability to install or delete licenses and stations (including the one running), also to install, reinstall, or upgrade the platform dist file and/or modules, and to start, re-start, or stop a station.
      • Admin - Full access. This includes all user-level platform operations, plus the ability to configure host TCP/IP settings and dial-up configuration, change platform authentication, change platform daemon HTTP port, change host date/time settings, use the File Transfer Client, and reboot the host.
    2. Digest platform authentication provides only full level platform login access, using a single platform user account. With Digest platform authentication, there is no linkage between Windows OS user accounts and the platform administrator.

If Basic authentication does not work, then Digest authentication must be used. To enable digest authentication, do the following:

  1. Using Notepad or WordPad, open the daemon.properties file located in C:\niagara\[release]\daemon folder
  2. Add the following lines to the end of the file: installFlag=doc authtype=digest/file user=[username] (where you select the username) password=[password] (where you select the password) stationIsAdmin=true
  3. Save, then close the file
  4. Restart the platform daemon (Start > Programs > Vykon AX Supervisor > Install Platform Daemon)
  5. Launch Workbench AX, then open the platform using the username and password you provided in step 2.

Consult the Niagara AX Platform Guide for more information.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 2742
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.