Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

The I/A Series G3 Modbus TCP slave device is unable to establish communications with a Modbus client requesting a unit identifier of 255.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • The I/A Series G3 Modbus TCP slave device is unable to establish communications with a Modbus client requesting a unit identi...
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • WaynePeters
    WaynePeters
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1737 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

The I/A Series G3 Modbus TCP slave device is unable to establish communications with a Modbus client requesting a unit identifier of 255.

Picard Product_Support
‎2018-09-11 06:30 AM

Issue

The I/A Series G3 Modbus TCP slave device is unable to establish communications with a Modbus client requesting a unit identifier of 255.  The ENC/JACE rejects the message because the Modbus TCP slave device address can only be configured with a value between 1 to 247.

Environment

I/A Series G3 (all versions)

Cause

The Modbus TCP slave device address can only be configured with a value between 1 to 247 and Workbench will generate an exception if a value outside this range is entered and saved.

Per the Modbus TCP standard, the Modbus TCP/IP Application Data Unit (ADU) takes the form of a 7 byte header (transaction identifier, protocol identifier, length field, and unit identifier) plus the protocol data unit (function code + data).

The 7 byte MBAP header includes the following fields:

  • Transaction/invocation Identifier (2 Bytes): This identification field is used for transaction pairing when multiple messages are sent along the same TCP connection by a client without waiting for a prior response.
  • Protocol Identifier (2 bytes): This field is always 0 for Modbus services and other values are reserved for future extensions.
  • Length (2 bytes): This field is a byte count of the remaining fields and includes the unit identifier byte, function code byte, and the data fields.
  • Unit Identifier (1 byte): This field is used to identify a remote server located on a non TCP/IP network (for serial bridging). In a typical Modbus TCP/IP server application, the unit ID is set to 0 or 0xFF (255), ignored by the server, and simply echoed back in the response.

Resolution

The I/A Series G3 Modbus TCP slave device address can only be configured with a value between 1 to 247 and Workbench will generate an exception if a value outside this range is entered and saved.  The workaround is to configure the value as follows.

  1. Right click on the ModbusTcpSlaveNetwork and view the ModbusTcpSlaveDevice objects.
  2. Right click on the ModbusTcpSlaveDevice object and select Pin Slots.
  3. Select the Device Address slot to pin ... select OK,
  4. Create a NumericWritable and set the value to 255.
  5. Link the output of the NumericWritable to the Device Address.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 15345
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.