Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

TC300 Series Networking Digital Fan Coil Thermostat - Modbus Protocol Documentation

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • TC300 Series Networking Digital Fan Coil Thermostat - Modbus Protocol Documentation
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
8860 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

TC300 Series Networking Digital Fan Coil Thermostat - Modbus Protocol Documentation

Picard Product_Support
‎2018-09-10 11:04 AM

Last Updated: Crewman ContentModerator ‎2025-09-25 03:06 AM

Issue

TC300 Series Networking Digital Fan Coil Thermostat - Modbus Protocol Documentation

Product Line

Field Devices

Environment

TC300 Series Digital Fan Coil Thermostats

Cause

Modbus protocol information is needed in order to perform Modbus integration to the TC300 Series Digital Fan Coil Thermostats.

Resolution

The TC303 thermostats come with the option of Modbus communication for both 2- and 4-pipe configurations. Modbus is an open, widespread and well established serial communication protocol used within building automation. The support of Modbus communication allows simple integration of the TC303 thermostats to a building management system, using standard Modbus serial communications. The following models provide support for Modbus connectivity:

  • TC303-3A2LM
  • TC303-3A4LM
  • TC303-3A2DLMS
  • TC303-3A4DLMS
  • TC303-3A2DPMS
  • TC303-3A4DPMS

The TC303 thermostats communicate as a Modbus RTU slave device over a serial RS-485 connection, allowing for the transfer of real time data. Thermostats manufactured from November 2018 (2018-W44-4)* onward can be configured to communicate at 9600 (default) or 4800 bps. The communication parameters for TC-300 thermostats manufactured prior to this date cannot be adjusted and are fixed as follows:

  • 4800bps Baud Rate
  • 8 Data Bits
  • Odd Parity
  • 1 Stop Bit

The actual Modbus address of the thermostat can be set for each individual device on the RS-485 network. The address is defined via the parameter menu on the thermostat itself. The address range available is from 01 to 32 and is defined under menu item 04 of the parameter settings.

For full details on this, other parameter setting options available and Modbus communications parameters/registers, please refer to the Installation Instructions. 

Connection to the RS-485 network is made via dedicated terminals on the back of the thermostat and marked A (+) and B (-).

 

TC300 Series Digital Fan Coil Thermostat Installation Instructions

TC300 Series Modulating Fan Coil Thermostat Installation Instructions

 

* Note - The Installation Instructions have not been updated to include the information that thermostats manufactured from November 2018 (2018-W44-4) onward can be configured to communicate at 9600 (default) or 4800 bps. 

Labels (1)
Labels:
  • Field Devices
Tags (1)
  • Find more articles tagged with:
  • 7553
Was this article helpful? Yes No
100% helpful (4/4)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.