Issue
Does TAC Vista Support MySQL Server?
Product Line
TAC Vista
Environment
- TAC Vista
- MySQL
Cause
User may wish to integrate TAC Vista with a MySQL installation for access to data or reporting.
Resolution
TAC Vista can not support MySQL Server. It only supports various types of Microsoft SQL Servers.
For details, please refer to the compatibility matrix which is available on Exchange Extranet, or refer to Software and Firmware compatibility matrix for older versions of I/NET, Vista, Andover Continuum, Sa....