Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Security Expert HID OSDP Reader LED Color Configuration

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Security Expert HID OSDP Reader LED Color Configuration
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Alan_Wood
    Alan_Wood

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
2 Likes
7320 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Security Expert HID OSDP Reader LED Color Configuration

Alan_Wood Leader
‎2023-08-07 10:10 PM

on ‎2023-08-07 10:10 PM

Issue

Tips for Configuring HID OSDP Reader LED Colors

Product Line

EcoStruxure Security Expert

Environment

EcoStruxure Security Expert
OSDP Reader

Cause

Additional tips for configuring OSDP Reader LED Colors

Resolution

The Configuring LED Colors section of AN-254 Configuring OSDP Readers in Security Expert  details the basic steps for LED configuration.

This article details some additional areas of the HID reader setup and Security Expert configuration that may be useful when configuring the LED colors.

 

Note: The steps in this article are specific to an HID Signo RP10 Reader BLE and may not apply to other HID reader models or other brands of OSDP readers.

 

    1. Upgrade the Reader firmware to the latest version. Earlier versions of the reader firmware would not correctly allow LED control. The Bluetooth option allows the configuration of the reader using the HID Reader Manager App. For detailed information see HID Reader Manager App Information

      Note: To use the HID Reader Manager App to configure a reader, the Security Technician or Security Installer needs to create and register an account with HID. The Reader Manager Administrator for your organization or company needs to enroll this new account using the Reader Manager Service and issue an invitation code and key authorization for this and other readers. The Security Technician can then verify the key authorization has been received in the HID Reader Manager app.

      Detailed instructions for all of this are included in the HID Reader Manager App Information URL listed above.

       

      HID Reader Manager App Firmware snapshots

      HID Reader Firmware Upgrading.png

      HID Reader Firmware Version.pngHID Reader Firmware Upgrade Successful.png

       

       

       

    2. In the HID Reader Manager App, change the Reader Options for LED color to "Host Controlled" in 2 places. The reader must be controlled by the Security Expert controller.

      1. Credential Reader AV

        Credential Read AV Host Controller.png

      2. LED Idle Color

        LED Idle Color Host Controller.png

    3. Ensure that the firmware for the following hardware is upgraded to these versions or greater in order for LED Color Output to work.

      • Security Expert 4.3.308.46

      • SP-C 2.08.1234

      • MRDM2 1.2.590

    4. In Security Expert the Outputs to control the LEDs need to be manually created.

      Programming> Outputs> Add

      A pop-up asking to Invert Output will display, select 'No' when prompted

      Invert Output.png

      Output 3 (GreenLED Port 1)

      Output 4 (Red LED Port 1)

      Output 6 (Green LED Port 2)

      Output 7 (Red LED Port 2)

       

      Name the Outputs whatever is appropriate

      Example: 

      GreenLEDPortON

      RedLEDPortOff

    5. LED Colors

      The default LEDs are Blue when Idle and Green when active.

      As an example, the LED colors will be changed to Red when Idle and Green when Active.

      Color Options:

      OSDP LED Color Options.png

       

      1. Set the colors for both Red(idle) and Green(active) in the Security Expert Output Command Window for the newly created outputs

        RedLEDPortOff

        RedLED Port Off Output.png 

        GreenLEDPortOn

        GreenLED Port On Output.png

      2. Update the modules and wait for about 15 seconds before activating the output to test.

        Just saving the updated command setting doesn't work, the module must be updated.

         

      3. Activate the GreenLEDPort1 - the color should change to what the output was set to in the command. In this case, green.

        Deactivate goes back to Off (idle) Red.

        GreenLEDPort1 = On State

        RedLEDPort1 = Off State

         

        Note: The Off state if left at the default of Blue can't be used with the On state of custom(non-default). Both Outputs must be specified in the command window for the colors to work together.

         

        Example: If the OFF state is left at the default of blue and the color of the ON state is set in the command window and Activated, the LED color will change to what it is set to(green), but when deactivating the Off(idle) output it will not turn blue.

Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (5)
  • Find more articles tagged with:
  • AdamSteele25
  • AlanWood23
  • colors
  • OSDP
  • reader
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.