Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

SQL error the transaction log for the database 'tempdb' is full.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • SQL error the transaction log for the database 'tempdb' is full.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support
  • AbeMeran
    AbeMeran

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
12072 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

SQL error the transaction log for the database 'tempdb' is full.

Picard Product_Support
‎2018-09-10 08:34 PM

Issue

SQL error: [Microsoft][ODBC SQL Server Driver][SQL Server]The transaction log for database 
'tempdb' is full. To find out why space int he log cannot be reused, see the log_reuse_wait_desc
column in sys.databases

Product Line

Andover Continuum

Environment

SQL Server

Cause

Low disk space or unreasonably low maximum size for tempdb database growth.

Resolution

SQL Server allocates a database called tempdb, primarily for worktable / #temp table usage. Sometimes, you will encounter a transaction log full error

 
Causes 
 
Usually, tempdb fills up when you are low on disk space, or when you have set an unreasonably low maximum size for database growth. 
 
Many people think that tempdb is only used for #temp tables. When in fact, you can easily fill up tempdb without ever creating a single temp table. Some other scenarios that can cause tempdb to fill up: 

  • any sorting that requires more memory than has been allocated to SQL Server will be forced to do its work in tempdb; 
     
  • if the sorting requires more space than you have allocated to tempdb, one of the above errors will occur; 
     
  • DBCC CheckDB('any database') will perform its work in tempdb -- on larger databases, this can consume quite a bit of space; 
     
  • DBCC DBREINDEX or similar DBCC commands with 'Sort in tempdb' option set will also potentially fill up tempdb; 
     
  • large resultsets involving unions, order by / group by, cartesian joins, outer joins, cursors, temp tables, table variables, and hashing can often require help from tempdb; 
     
  • any transactions left uncommitted and not rolled back can leave objects orphaned in tempdb; 
     
  • use of an ODBC DSN with the option 'create temporary stored procedures' set can leave objects there for the life of the connection.

 
Short-term fix 
 
Restarting SQL Server will re-create tempdb from scratch, and it will return to its usually allocated size. In and of itself, this solution is only effective in the very short term; assumedly, the application and/or T-SQL code which caused tempdb to grow once, will likely cause it to grow again. 
   
Long-term prevention 
 
Here are some suggestions for maintaining a healthy tempdb: 

Make sure that tempdb is set to autogrow -- do *NOT* set a maximum size for tempdb. If the current drive is too full to allow autogrow events, then buy a bigger drive, or add files to tempdb on another device (using ALTER DATABASE) and allow those files to autogrow. You will need at least one data file and at least one log file in order to avoid this problem from halting your system in the future. 

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 7751
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.