Issue
Is it possible to run a Forta series actuator on 24VDC?
Environment
TAC Forta series actuators:
M300
M310
M400
M750
M800
M1500
M3000
Cause
The TAC Forta series actuators older documentation suggests it can only be run on 24VAC only.
Resolution
The TAC Forta series actuators can run on 24VAC +/- 25% or 24Vdc +/- 10%.
For more specific details on tolerances, please see the data sheet for each product.