Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Modbus write command setup and timing

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Modbus write command setup and timing
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Dave_Shore
    Dave_Shore
  • DavidChild
    DavidChild
  • sesa139513
    sesa139513
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3506 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Modbus write command setup and timing

Picard Product_Support
‎2018-09-07 10:58 AM

Issue

Modbus write command setup and timing

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Automation Server (AS, AS-P, AS-B)
  • Building Operation Enterprise Server (ES)

Cause

The Modbus value keeps being sent to a Modbus register (when write code 06 or 16 used)

Resolution

Control of the write timing is via the binding to the Modbus point within the Modbus network.

  • If the Communication type is set to "Periodic" then the value will be sent based on the Period Communication Interval.
  • If the Communication Type is set to "Change of Value" then the value will only be written when the value changes by this amount.

The Re-transmit Interval should also be considered, as the register will also be written to based on this timing value, regardless as to whether it has changed or not. This value may need to be increased if the value should not be re transmitted apart from when the value changes.

Up to v1.3

v1.4 and later

Some Modbus devices get over these sort of issues by having a mode that can be set so that re-transmission of the same value is ignored, as the example below

NOTE
Block (Batch, Multiple) Writes are not supported (correct as 2020 11 01 and up to v3.2) Although they are used to write to 32, 48 & 64 bit Register types (so "Write Multiple Registers" packets will be seen when writing to 32, 48 or 64 bit registers) 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (13)
  • Find more articles tagged with:
  • 14890
  • 802
  • change of value
  • code 06
  • code 16
  • cov
  • DavidShore20
  • enhancement
  • LastTouch
  • modbus
  • OnChange
  • periodic
  • write
Was this article helpful? Yes No
100% helpful (3/3)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.