Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Max Info Frames attribute in a Continuum BACnet controller

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Max Info Frames attribute in a Continuum BACnet controller
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • sesa119747
    sesa119747
  • Product_Support
    Product_Support
  • sesa101527
    sesa101527

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
6640 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Max Info Frames attribute in a Continuum BACnet controller

Picard Product_Support
‎2018-09-06 02:59 PM

Last Updated: Administrator DavidFisher Administrator ‎2019-06-18 02:10 PM

Issue

What is the purpose of the Max Info Frames attribute in a Continuum BACnet controller?

Product Line

Andover Continuum

Environment

  • BACnet MS/TP, MaxInfoFrames
  • Optimizing MSTP

Cause

Information on the Max Info Frames function.

Resolution

The Max Info Frames setting on the BACnet controller object editor specifies how many messages that the controller can send out to other controllers when it has the token on the network. For instance, a B3 controller has a default of 2 for this setting. If it receives the token on the MSTP network and it has 5 COV or Event notifications to send to other controllers or workstations, it will send the first 2, and wait until it gets the token the next time around and send 2 more, etc.

The BCX controller has a default of 8 for Max Info Frames.

This setting is changeable through the BACnet controller editor, however care should be taken not to increase it to too large a number. The larger the setting, the more time that particular controller can hold the onto the token, which in turn denies other controllers on the network the capability of sending out their data in a timely manner. It should only be adjusted if there is a definite need for increased messaging, but on the MSTP network it is not recommended to go above 10, although we do not limit the value.

In a Cyberstation Version 1.8 or above the setting can be made on the details page of the BACnet controller device editor.

If adjustment of this parameter is done using any Cyberstation prior to version 1.8, the setting will not stay at the new value after a controller reload from the Infinity side, it will revert to it's default. You will need to create a PE program in the controller to set this parameter to the desired value if it is reloaded. The program should be autostart and fallthru, and use the "Writeproperty" keyword to set the parameter. The syntax should be as follows:

Line SetMaxInfo
  WriteProperty ("Full Bacnet path name of controller", MaxInfoFrames, "New Value")
Stop
Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 2556
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.