Issue
How to make a graphic page pop up in Vista Workstation when an alarm occurs.
Environment
Vista Workstation
Cause
Steps of making a graphic page pop up in Vista Workstation when an alarm occurs may not be very obvious to many users.
Resolution
- Locate the alarm object in Workstation.
- Right click on that alarm object and select "Properties"
- In the "Properties" window, select "Video/Graphic" tab.
- In the "Linked graphic" text box, browse to your graphic object and click "OK" to save it.
- Check "Show graphic automatically".
This is also discussed in the TAC Administering Manual in Chapter 7.