Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Is there a process to downgrade an ENC-410 or ENC-520?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Is there a process to downgrade an ENC-410 or ENC-520?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa116873_brid
    sesa116873_brid
  • WaynePeters
    WaynePeters
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1566 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Is there a process to downgrade an ENC-410 or ENC-520?

Picard Product_Support
‎2018-09-06 01:27 PM

Issue

Attempting to downgrade the ENC-410 or ENC-520 using the Commissioning Wizard can corrupt the ENC file system making the ENC become unusable.

Environment

I/A Series G3, ENC-410, ENC-520

Cause

Attempting to downgrade the ENC-410 or ENC-520 using the Commissioning Wizard can corrupt the ENC file system making the ENC become unusable.

Resolution

Downgrading from one software release to an earlier release can present compatibility problems. This applies particularly to QNX-based ENCs, as binaries for the (QNX) OS are included in dist files.  However, at times it may be necessary to install an older release onto a ENC, or to restore a ENC to a known good state. To downgrade a ENC, or otherwise “wipe it clean to start over,” a clean distribution file must first be installed.  The following procedure is also detailed in the Niagara AX Platform Guide included with the G3 software.

Installing a clean dist will wipe the file system and install an appropriate version of Niagara platform daemon, resetting the unit to a “near factory state.” Only the following settings are preserved:

• TCP/IP settings
• license files
• brand.properties

All other data is removed from the file system, including station bog files, Px files, modules, etc. In addition, a clean dist restores the factory-default platform credentials and port (3011).  Therefore before installing a clean dist file, make sure to backup station files plus any other modules on the ENC you wish to keep.

Remember, that a “Station Backup” creates a dist file that (when restored) includes the same level of software installed at backup time, so instead of (or in addition to) this type of backup, you may wish to use the Station Copier.

Note that after installing a clean dist, you must recommission the ENC, using the Commissioning Wizard.

---

To downgrade a QNX-based ENC from any G3 3.x build to an earlier release:

Step 1: Before installing a clean dist file, make sure you have backed up the station files plus any other data and modules on the ENC you wish to keep.

Step 2: Start G3 3.x Workbench and open a platform connection to the ENC.

Step 3: Open the Distribution File Installer and click Cleaning button for the !/cleanDist directory.

Step 4: Select the appropriate clean dist file for the platform and install.  The file system clean will take a few minutes, then the ENC will automatically reboot. Wait for the reboot to complete.

Note: After reboot from a clean dist install, the ENC is using default platform credentials and port (3011).

Step 5: Re-install the software versions to the ENC. Use a version of Workbench that runs the same software versions that you want on the UNC, and use the platform Commissioning Wizard to install the desired software build. For details, refer to the section “About the Commissioning Wizard” in the JACE NiagaraAX Install and Startup Guide.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 5876
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.