Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Integrating EBO with ESMI Fire Detection Panel

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Integrating EBO with ESMI Fire Detection Panel
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • PeterEdvik
    PeterEdvik
  • Jonas_Brissman
    Jonas_Brissman
  • SharlinaRe
    SharlinaRe

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
5009 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Integrating EBO with ESMI Fire Detection Panel

PeterEdvik Champion
‎2021-11-24 02:24 AM

on ‎2021-11-24 02:24 AM

Issue

Would like to monitor and control points and alarms from an ESMI Fire Detection Panel in EBO.

Product Line

EcoStruxure Buildning Operation

Environment

  • Building Operation Automation Server Premium (AS-P)
  • ESMI Fire Detection Panel

Cause

The integration between ESMI Fire Detection Panel and EBO enables the user to visualize and operate ESMI Fire detection systems effectively from graphics in EBO.

Resolution

The interface between the ESMI Fire panels and EcoStruxure Building Operation (EBO) is handled by the AS EN54 FIRE SmartDriver. The event and command information is sent/received by the Fire panel using RS-485 communication to/from the AS-P using the SmartDriver.

 

This resolution is in three steps:

  1. Enable communication via RS485 (INFO protocol in Fire panel)
  2. Use the AS EN 54 Fire Configurator to create the layout for EBO
  3. Install/configure the SmartDriver and create the Fire graphics in the AS-P

 

Step 1 - Enable communication via RS485 (INFO protocol in Fire panel)

This video shows how to enable communication from an ESMI Fire panel and an AS-P over RS485. This is a prerequisite for using the Fire SmartDriver in the AS-P.

 

 

Step 2 - Use the AS EN 54 Fire Configurator to create the layout for EBO

This video will give you a quick introduction to the AS EN54 Fire Configurator. The AS EN54 Fire Configurator is a Windows application that imports floor plans and configuration files to create the EBO interface, devices, points, alarms and graphics.

 

 

Step 3 - Install/configure the SmartDriver and create the Fire graphics in the AS-P

This video shows how to connect an EBO SmartX Server to an Esmi Sense Fire detection panel (FDP).
And how to create and edit the Fire graphics in the EBO SmartX Server, The fire graphics provide the user interface to visualize and operate Esmi Fire detection systems.

 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (3)
  • Find more articles tagged with:
  • JonasBrissman21
  • PeterEdvik21
  • SharlinaRenwall21
Was this article helpful? Yes No
100% helpful (4/4)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.