Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Importance of correct selection / installation of Satchwell 3-port Valve Body to provide Mixing function or Diverting function.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Importance of correct selection / installation of Satchwell 3-port Valve Body to provide Mixing function or Diverting functio...
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2469 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Importance of correct selection / installation of Satchwell 3-port Valve Body to provide Mixing function or Diverting function.

Picard Product_Support
‎2018-09-07 11:14 PM

Last Updated: Crewman ContentModerator ‎2025-09-25 02:48 AM

Issue

Importance of correct selection / installation of Satchwell 3-port Valve Body to provide Mixing function or Diverting function.

Environment

Satchwell 3-port Valve Body to provide Mixing function or Diverting function in heating or cooling circuit.

 

Satchwell MB, MBF, MJF, MZ, MZF, MZX

Cause

Incorrect selection / installation  of Satchwell 3-port Valve Body to provide Mixing function or Diverting function may result in poor control, damage to the Valve Body, damage to the Valve Actuator or damage to the hydraulic installation.

Resolution

  1. Determine which of the following types of hydraulic circuit the Satchwell 3-port Valve Body is to be installed in.
    1. Constant Temperature Variable Volume (CT) circuit e.g. AHU Heating / Cooling Coil or Calorifier Coil 
    2. Variable Temperature Constant Volume (VT) circuit e.g. Radiator System
  2. For Constant Temperature circuit application install Satchwell 3-port Valve Body as follows :-
    1. MJF, MZ, MZF, MZX install in RETURN pipework.
      Port 3 - Connect to Bypass (IN)
      Port 2 - Connect to Coil Return (IN)
      Port 1 - Connect to System Return (OUT)
    2. MB, MBF install in RETURN pipework.
      Port 3 - Connect to Bypass (IN)
      Port 2 - Connect to Coil Return (IN)
      Port 1 - Connect to System Return (OUT)
      OR
    3. MB, MBF may alternatively be installed in FLOW pipework
      Port 3 - Connect to Bypass (OUT)
      Port 2 - Connect to Coil Flow (OUT)
      Port 1 - Connect to System Flow (IN)
  3. For Variable Temperature circuit application install Satchwell 3-port Valve Body as follows :-
    1. MJF, MZ, MZF, MZX install in FLOW pipework.
      Port 3 - Connect to Bypass (IN)
      Port 2 - Connect to Boiler Flow (IN)
      Port 1 - Connect to System Flow (OUT)
    2. MB, MBF install in FLOW pipework.
      Port 3 - Connect to Bypass (IN)
      Port 2 - Connect to Boiler Flow (IN)
      Port 1 - Connect to System Flow (OUT)
      OR
    3. MB, MBF may alternatively be installed in RETURN pipework
      Port 3 - Connect to Bypass (IN)
      Port 2 - Connect to System Return (IN)
      Port 1 - Connect to Boiler Return (OUT)

N.B.

It should be noted that the alternative installation methods are valid for the MB and MBF Valve Bodies due to the ROTARY SHOE construction of the MB and MBF

Similarly it should be noted that the alternative installation methods are not valid for the MJF, MZ, MZF and MZX Valve Bodies due to the PLUG AND SEAT construction of the MJF, MZ, MZF and MZX .

Failure to install MJF, MZ, MZF and MZX Valve Bodies correctly in the pipework may result in VALVE VIBRATION in the pipework caused by WATER HAMMER 

 

INSTALLATION OPTIONS - MJF, MZ, MZF and MZX

3-PORT PLUG AND SEAT VALVES MAY BE INSTALLED TO MIX IN THE FLOW

VALVE BODIES USE TWO “IN” PORTS (Ports 2 & 3) AND ONE “OUT” PORT(Port 1)

 

3-PORT PLUG AND SEAT VALVES MAY BE INSTALLED TO DIVERT (BY MIXING) IN THE RETURN

VALVE BODIES USE TWO “IN” PORTS (Ports 2 & 3) AND ONE “OUT” PORT(Port 1)

 

INSTALLATION OPTIONS - MB, MBF 

3-PORT ROTARY SHOE VALVES MAY BE INSTALLED TO MIX IN THE FLOW USING TWO “IN” PORTS (Ports 2 & 3) AND ONE “OUT” PORT (Port 1)

3-PORT ROTARY SHOE VALVES MAY BE INSTALLED TO MIX IN THE RETURN.USING ONE “IN” PORT (Port 1) AND TWO “OUT” PORTS (Ports 2 & 3))

3-PORT ROTARY SHOE VALVES MAY BE INSTALLED TO DIVERT IN THE RETURN USING TWO “IN” PORTS (Port 2 & 3) AND ONE “OUT” PORT (Port 1)

3-PORT ROTARY SHOE VALVES MAY BE INSTALLED TO DIVERT IN THE FLOW USING ONE “IN” PORT (Port 1) AND TWO “OUT” PORTS (Port 2 & 3)

 

RELATED INFORMATION - DIVERTING IN THE FLOW

It should be noted that some manufacturers produce 3-Port Plug and Seat Valve Bodies specifically designed to DIVERT in the FLOW.  Such Valve Bodies have 1 IN Port and 2 OUT Ports

 

Please check the latest catalog for current equipment.


 

Labels (1)
Labels:
  • Field Devices
Tags (1)
  • Find more articles tagged with:
  • 5074
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.