Issue
How many Video Servers can be used with CyberStation?
Environment
CyberStation
Cause
The answer to this question depends on the revision of CyberStation that is being used.
Below is a list of CyberStation revisions and what quantity of Video Servers they support.
Resolution
| CyberStation Revision | Quantity of Video Servers | |
|---|---|---|
| Below Revision 1.60 | 0 | |
| Revision 1.60 to 1.71 | 10 | |
| Revision 1.73 to 1.74 w/o SP2 | 50 | |
| Revision 1.74 SP2 to 1.82 | 100 | |
| Revision 1.90 and above | unlimited |