Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How do I trigger my fallthru script program to run?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How do I trigger my fallthru script program to run?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa139513
    sesa139513
  • DavidFisher
    DavidFisher
  • PaulFr
    PaulFr
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2771 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How do I trigger my fallthru script program to run?

Product_Support
‎2018-09-06 03:11 PM

Issue

Looping script programs continuously loop around the code, but a fallthrough needs a trigger to start it running and will stop at the end. How is this configured.

Environment

Script programs set as Fallthrough in an AS or ES

Up to Release 1.3

Cause

Plain English used Triggers in points to start a program, these do not exist in an AS or ES Binary value, so what is used to start the program running?

Resolution

Once a script program has been written, checked and  saved as a Flow Type "Fallthru", you can then edit the bindings.

In the bindings use the variable called "Restart" a binary value to bind to the triggering point/ value which should also be Binary.

This object can then be triggered on the required event to start the program, which will then execute the code and stop at the end awaiting the next restart.


When you Bind a Digital Value to a Scrip program, you may get an error message like the one here:

By Default, a Digital Value has no Configuration Settings defined. Enter 0 and 1 for the binary states and then performing your binding to the Program alleviates the error message. 

Note: This functionality operates for versions up to Release 1.3. From Release 1.4 the Restart attribute is read only showing the restart status from the program and does not allow a point / value to be bound to this flag.

In Release 1.4 a looping program will need to be used checking the state of the trigger point and action accordingly.

 

Note: in newer releases e.g. 1.7, 1.8 and above, triggers are now supported and you can bind directly to the Trigger attribute of the program, each change of the bound point will trigger the script to run.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (4)
  • Find more articles tagged with:
  • 8355
  • editing
  • property
  • scripts
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.