Issue
A panel unit’s title (description) in a DMS database needs to be updated. How can this be done using OPRIF?
Product Line
TAC IA SeriesEnvironment
- DMS Operator Interface (OPRIF)
- All revisions of DMS 35, DMS 350A, and DMS 3500
Cause
Equipment naming has changed, requiring updates to the DMS database to maintain consistency.
Resolution
- Access the Message Text Table in OPRIF.
- Locate the Panel Unit Descriptor Message that needs modification.
- Use the following steps:
- Cursor down to the descriptor requiring modification.
- Press the “=” key.
- Type the new text for the title.
- Press Enter to save changes.
- For detailed instructions, refer to Chapter 4 – “Setting Up Tables” in the DMS Operator Interface User’s Guide (F-25467).