Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

General recommendations for LonWorks system architecture

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • General recommendations for LonWorks system architecture
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1997 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

General recommendations for LonWorks system architecture

Product_Support
‎2018-09-06 03:24 PM

Last Updated: ContentModerator Explorer ‎2025-08-11 04:01 AM

Issue

What are the general recommendations for LonWorks system architecture?

Product Line

TAC Vista, TAC IA Series

Environment

  • LNS database
  • LonWorks network
  • Vista Server
  • I/A Series MNL

Cause

Understanding the different communication speeds and optimal site design can lead to improved performance of LON traffic on a network.

Resolution

There are three levels supported by LonWorks.

  1. TCP/IP
  2. 1.25mbs high speed backbone
  3. 78Kbs FTT-10 level

Our recommendation is to maximize the use of TCP/IP, minimize the use of the 1.25mbs high-speed backbone and use a tiered structure of 78Kbs LON segments. The IP provides high-speed data transfer, which is good. The 1.25mbs high-speed bus works fine, but it has a number of special requirements that must be adhered to for proper operation. The flexibility of this 1.25mbs network is limited for the expansion of new Lonworks segments, whereas the TCP/IP is more in line with current building infrastructure making it easier to expand the LonWorks system.

In the TCP/IP there are two options that allow for better communications.

  1. Standard TCP/IP configuration that will work well for most middle-sized networks. This is standard with NL220 or Lonmaker installations
  2. Orion Stack is an improvement on the standard TCP/IP and can poll multiple values at one time helping improve the TCP/IP response on large networks. More information in setting up an Orion stack improved TCP/IP LonWorks network.
Labels (1)
Labels:
  • TAC Vista
Tags (3)
  • Find more articles tagged with:
  • 1173
  • PeterLarsen19
  • PeterLarsen23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.