Issue
Integration between Power Monitoring Expert (PME) and EcoStruxure Building Operation (EBO) fails due to default security settings that prevent embedding external web content.
Product Line
EcoStruxure Building Operation
Environment
- Building Operation WebStation
- PME Web Applications
Cause
By default:
- PME restricts other applications from embedding its web content.
- EBO blocks external web content from being embedded in its UI.
To enable integration, both systems must be configured to allow embedded content.
Resolution
✅ Enable External Content in EBO WebStation
- Log into Building Operation Workstation.
- Navigate to:
Tools > Control Panel > Security and Communication > Security Settings - Under WebStation, check the box:
✔ Enable external content to be embedded in WebStation
✅ Authorize EBO to Embed PME Web Applications
- Open PME Web Applications.
- Go to:
SETTINGS > Security > Authorized Hosts - Add the Building Operation server URL to the Hosts That Can Frame list.
Example:https://localhost:446 - Click Save.
- Reset IIS (Internet Information Services) on the PME server to apply changes.
Notes
- Ensure both systems are updated to compatible versions.
- Use secure URLs (HTTPS) when configuring host permissions.
- Resetting IIS may cause temporary downtime—schedule accordingly.