Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Drayton DC2100 series Optimiser / Compensator Controller - Reset to Default Values procedure.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Drayton DC2100 series Optimiser / Compensator Controller - Reset to Default Values procedure.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3659 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Drayton DC2100 series Optimiser / Compensator Controller - Reset to Default Values procedure.

Picard Product_Support
‎2018-09-10 05:21 AM

Issue

DC2100 series Optimiser / Compensator Controller requires resetting to default values due to exposure to electrical corruption.

Environment

DC2100 series Optimiser / Compensator Controller installed to control Variable Temperature Mixing Valve, Boiler/s, Pumps etc.

2100H

DC

2100

Cause

DC2100 series Optimiser / Compensator Controller has been exposed to electrical corruption.

Resolution

DC2100 series Optimiser / Compensator Controller may be reset to default values as follows :- 

  1. Isolate power to Controller.
  2. Open Door of Controller.
  3. Locate PCB on rear of Controller Door.
  4. Locate pair of Steel Pins (marked PL1) on PCB.
  5. Link out pair of Steel Pins for 10 seconds approx.
  6. Remove Link.
  7. Close Door of Controller.
  8. Reinstate power to Controller.
  9. Re-programme Controller.

Re-programming procedure for the DC2100 series Optimiser / Compensator Controller may be viewed here.

Should the above reset to default values procedure fail to enable the DC2100 series Optimiser / Compensator Controller to be re-programmed then replacement of the Controller may need to be considered.

POSSIBLE REPLACEMENT 

The most common control application to which theDC2100 series Optimiser / Compensator Controller may be applied comprises the following combination of inputs and outputs. 

Outside Air Temperature Sensor

Inside Air Temperature Sensor

Compensated Heating Temperature Sensor

Variable Temperature Heating Circuit Valve Actuator

Boiler/s (2 maximum)

H W S On/Off output (independent)

Should such inputs and outputs be confirmed then the DC1100 Optimiser / Compensator may be installed in place of the DC2100 series Optimiser / Compensator Controller.

Details of the DC1100 Optimiser / Compensator Controller may be viewed here.

Drayton A7xx series Sensors connected to the DC2100 Optimiser / Compensator Controller are compatible with the DC1100 Optimiser / Compensator Controller and may therefore be retained.

N.B.

It should be noted that where a DC2100 series Optimiser / Compensator Controller is included in an installation of a more complex nature then an alternative solution utilizing different products may need to be considered

In such installations not only will the DC2100 series Optimiser / Compensator Controller need to be replaced but its associated Sensors will also need to be replaced.

Resolutions to such installations may best be determined following a review of the control system installed by a member of the local Schneider Electric office.

Labels (1)
Labels:
  • Field Devices
Attachments
Tags (1)
  • Find more articles tagged with:
  • 6931
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.