Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

Conversion process for taking small numbers in I/NET Seven to Large numbers in I/NET Seven

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Conversion process for taking small numbers in I/NET Seven to Large numbers in I/NET Seven
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Tom_Poovey
    Tom_Poovey
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1490 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Conversion process for taking small numbers in I/NET Seven to Large numbers in I/NET Seven

Picard Product_Support
‎2018-09-10 03:12 AM

Issue

Conversion process for taking small numbers in I/NET Seven to Large numbers in I/NET Seven

Environment

I/NET Seven rev 1.12 and above

Cause

The card number of the Prox cards are larger than 24000

Resolution

  1. Sort the Individuals list according to the Individual Number. Find out the lowest number in the list. In this example number 1 is the lowest card number.


     
  2. Look at the tenant editor to determine the Tenant Code/Facility code of the cards.


     
  3. Go into the Door Editor and verify the Bit Format of the Cards. In this case it is a standard 26-Bit Format.


     
  4. Verify in the door editor that the cards in this system are 26-Bit Wiegand. Then use the attached Excel spreadsheet (This is a ZIP File) to determine the Decimal number of the first card in the system (Card #1 Facility code 199) is 13041665. This number will become the source number in the Key card table.


     
  5. Create a Key card table like below, using the Source # that was determined in Step #3 above. Please note the Target # must be equal to the value of the Lowest Individual Number.


     
  6. Next unzip the supplied Windows SQL Script (BigCardConvert.exe).
    Please note that the SQL Script will ask for a Username and Password. These are the Username and Password used for the SQL in the DbCreate Editor.
  7. Once unzipped, double click the “EXE” file and this will convert all the existing card numbers into “Hex” numbers.
  8. After this process has completed, verify that the cards did in fact convert OK. Look at the lowest individual number the (“Source” card used the “Hex” and “Decimal” numbers) will be the same values determined in the Excel spread sheet.
  9. After verifying that all is OK, then delete the “Card Key Translation” table created to do this process.
Labels (1)
Labels:
  • TAC INET
Attachments
Hex XLS.ZIP
BigCardConvert.zip
Tags (1)
  • Find more articles tagged with:
  • 6220
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.