Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Control a dual duct VAV box with Xenta controllers

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Control a dual duct VAV box with Xenta controllers
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2519 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Control a dual duct VAV box with Xenta controllers

Picard Product_Support
‎2018-09-06 03:04 PM

Issue

How can I control a dual duct VAV box with Xenta controllers?

Environment

Xenta 102-AX

Dual Duct heating/cooling

Cause

The Xenta 102-AX is an application specific controller designed to vary the volume and outlet temperature of a single terminal unit. It does not, by default, control a dual duct, where a constant source of cold air and hot air and delivered in separate ducts.

Resolution

You could conceivably use a single Xenta 102-AX with the airflow pickup on the discharge of the box instead of the inlet. Then connect the hot deck damper as a 2-out PWM heat stage.

A more elegant solution is to use a pair of Xenta 102-AX controllers. One 102-AX is connected to the cool deck and setup normally. Either its heating airflow setpoint is set to match the cooling low flow or heating airflow is set to 0 if you wish the cool deck to shut off in heat. The "Effective Setpoint Source" must be set to "Norm of Heating and Cooling Setpoints" so that the setpoint sent to the hot deck controller will not bounce from heating to cooling when room conditions change. For this reason, it might be preferable to use an STR-202 so that there is no digital display to confuse the occupant.

The second 102-AX is connected to the hot deck, space temp is bound from the first and nvoeffectivesp is bound from the first to nvisetpoint of the second. Configure input 1 as a duct temp and connect a 4.7Kohm resistor from it to ground. This will simulate a duct temp of 110°F and keep it in warmup mode. As with the cool deck, you have a choice whether to set the warmup low flow to 0 or to some minimum position. Set your occupied setpoints to the same values as the cool deck controller. (It's actually using them in the setpoint calculation, but for simplicity's sake, set them the same. For a more complete description, consult the reference manual concerning nviSetpoint.)

You should also bind nvoOccupancyStatus from the cool box to nviOccCmd on the hot deck box. That way if someone puts the box in to after hours override, they'll both operate.

As mentioned before, the room sensor (STR-200/202/250) is connected to the cooldeck controller. You'll need to connect 3 conductors to a 1/8"TRS jack to the hotdeck controller in order to connect the MSTAT for calibration purposes. Otherwise you'll have to crawl into the ceiling to connect it.

This arrangement is based on having airflow sensors on the inlets of both the cold and hot deck.

Labels (1)
Labels:
  • TAC Vista
Tags (4)
  • Find more articles tagged with:
  • 2088
  • double
  • morning
  • thermostat
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.