Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

Continuum single user system database backup with SQL 2005 Express.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Continuum single user system database backup with SQL 2005 Express.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa119747
    sesa119747
  • Carl_Slack
    Carl_Slack
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2049 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Continuum single user system database backup with SQL 2005 Express.

Picard Product_Support
‎2018-09-06 02:45 PM

Issue

Continuum single user system database backup with SQL 2005 Express.

Environment

Continuum Cyberstation single user (SU)

Cause

Method to backup system database.

Resolution

Continuum single user system database backup with SQL 2005 Express.

Using SQL Express Management tool

  1. Right Click on the Continuumdb> Tasks>Backup
  2. Add a Destination where you want the .bak file to be located
  3. Click Ok

Using sqlcmd

With the limited release version of Continuum 1.82 and future 1.9x releases SQL 2005 Express will be the database platform that is used for Single User configurations.

Some of you may remember backing up databases in earlier versions of SQL from the windows command line and recall having to create a backup device in order to perform the backup operation. This is the case for backing up a database in the SQL 2005 Express version as well. 

  1. Open up the Windows command line and type in CD\ and press enter. This puts us at the root of the drive.
  2. Log on to the SQL 2005 server, by typing sqlcmd -Syourmachinename\sqlexpress and press enter. You should see 1> at this point. If you do not see the 1> prompt at this point, a few things could be going on. Make sure you type in your computer name without spaces following the -S switch. Another problem could be that your user logon doesn't have admin privileges. You need to have admin privileges to backup the database. 
  3. Once at the 1> create a backup device. Type EXEC sp_addumpdevice 'disk', 'MyDBbackup','c:\myTest.bak' and press enter, which should bring you to the 2> prompt
  4. At the 2> type in GO And press enter. This will create a device that we can now use to backup the database. The device should only need to be created once.
  5. Now that we have a device named MyDBbackup (you can name yours differently) and are at the 1> again, type in BACKUP database continuumdb TO MyDBbackup with init press enter and you should be at the 2> now type in GO
  6. You should have a backup of your database at the root of c:\ named mytest.bak It would be a wise idea to write down the name of the device you have created, since you can use the same device again. 
  7. Using the windows task scheduler, you can setup a task to backup your database automatically at the times you've specified in the task scheduler is an easy thing to do.
Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 3118
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.