Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Connecting a serial cable to a Xenta 5/7/9xx controller

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Connecting a serial cable to a Xenta 5/7/9xx controller
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
8916 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Connecting a serial cable to a Xenta 5/7/9xx controller

Product_Support
‎2018-09-07 12:37 AM

Last Updated: ContentModerator Explorer ‎2025-08-11 03:59 AM

Issue

Connecting a serial cable to a Xenta 5/7/9xx controller

Product Line

Satchwell MicroNet, TAC INET, TAC Vista

Environment

  • Xenta Servers
  • Xenta 511, 527, 555, 701, 711, 721, 731, 913

Cause

Xenta Servers have a service portal for use with HyperTerminal with a serial connection to the RS-232B port.

Resolution

  1. Connect a serial cable, Programming Serial Kit, part no. 0-073-0920-0, between the PC and the RS232 port B on the TAC Xenta.  For more information about the cable see Cable Guide OFL-3972.
  2. Go to Start/All Programs/Accessories/Communications/HyperTerminal, and open the HyperTerminal.
  3. In Connection Description Windows, type any name you like in the Name box.
  4. Click OK.
  5. In the Connect to window, choose the correct COM port that the RS-232 cable is using. If you do not know which COM port it is using.
  6. Go to your computer device manager. (Right click on “My computer” icon, and choose “Manage”. Then under “System Tools”, choose “Device Manager”.
  7. Find “Ports (COM & LPT)” and expend it
  8. Find the COM port number that is used by the RS-232 cable.
  9. Click OK.
  10. In the COM Properties window, type 9600 for “Bits per second”, 8 for “Data bits”, “Parity” is None, “Stop bits” is 1, and “Flow control” is None.
  11. Click OK.
  12. Options: you can save this setting for future use. Click on File Menu and Save.
  13. Press ENTER to activate the command prompt.
  14. Default username and password is both “root”. Type “root” and press ENTER for both the username and password.
  15. Type “setip” and press ENTER.

NOTE: Product support has also witnessed strange behavior with serial connections when certain laptops were not plugged into a power source or the Xenta Server was not grounded. If connection problems persist after the connection setting above are verified, make sure the Hyperterminal PC is plugged into a 120 vac power source.

Labels (3)
Labels:
  • Satchwell MicroNet
  • TAC INET
  • TAC Vista
Attachments
Tags (2)
  • Find more articles tagged with:
  • 1502
  • PeterLarsen20
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.