Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Configuring Default Gateways on both Ethernet Adapters on a JACE-8000/9000

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Configuring Default Gateways on both Ethernet Adapters on a JACE-8000/9000
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RandyDavis
    RandyDavis

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1205 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Configuring Default Gateways on both Ethernet Adapters on a JACE-8000/9000

Guinan RandyDavis Guinan
‎2025-02-20 04:58 PM

on ‎2025-02-20 04:58 PM

Issue

Incorrect Default Gateway setting may prevent communication with the JACE-9000

Product Line

TAC IA Series

Environment

I/A Series Jace 8000/9000

Cause

The Jace8000 and Jace9000 both have primary and secondary LAN adapters. Previously, Workbench prevented users from some invalid IP configurations, but current versions of Workbench, when connecting to a 9000 will allow invalid configuration in the default gateway.

Resolution

In the 9000, a user can set different default gateways for the Primary (en0) and Secondary (en1) ports. This should not be allowed on a single network device, and leads to unpredictable behavior when routing. Compare the location of the IPv4 Default Gateway in the TCP/IP Configuration of the Platform on a 9000:

 

EN0.png

 

EN1.png

 And the same page as seen in the 8000:

EN8000.png

In future versions, this will be changed, but users should avoid invalid configurations in the affected versions.

When configuring both LAN ports for use on a 9000, only enter a value for the default gateway field in one adapter. Leave the other intentionally blank. It does not matter which is given a default gateway and which is left blank.

Note: Sometimes, when an Adapter has the Default Gateway, you cannot connect to the other Adapter (despite correctly being on that Adapter's local subnet).
These symptoms can be triggered by the Ethernet "link" (active connection) toggling up or down.  The link state can change whenever:

  • the JACE is rebooted or power-cycled; and/or
  • the Ethernet switch ("hub")  is rebooted or power-cycled; and/or
  • the Ethernet cable(s) are un- or re-plugged (at either end).

In some cases, the symptoms can alleviated by toggling the Ethernet link state, in the ways listed above.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • RandyDavis25
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.