Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Changing the path of a Pinpoint active animation control image file

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Changing the path of a Pinpoint active animation control image file
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2360 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Changing the path of a Pinpoint active animation control image file

Picard Product_Support
‎2020-10-22 03:19 AM

Last Updated: Crewman ContentModerator ‎2025-09-01 03:34 AM

Issue

Is there a way to globally change the path of active animation controls so that each control does not have to be edited manually? Pinpoint graphics will be very slow to open if the image file is on a network drive that is no longer available.

Product Line

Andover Continuum

Environment

CyberStation

Warning

Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support Services for assistance.

Cause

A method to make the change globally in one operation is required system the design does not provide a way to do it.

Resolution

As of version 1.94 Continuum does not provide a mechanism to globally change the path of image files in active animation controls in Pinpoint.

This can be a problem when a large number of active animation controls have been created using a given path and the image files then need to be moved.

If the image files must be moved, every effort should be made to retain the path that was used in the controls, otherwise the path to the files will have to be manually changed in each active control that references the path in the graphic panel.

With the above said there is a way to go in the Graphic PIN file and change the path, it requires a hex editor such as HxD.

Using a hex editor the path for a control like this

Can be found and changed in the PIN file itself, like this...

*** Warning ***

Please note that the length of the new path string must be the same length (i.e. take up the same number of characters) as the original path string, otherwise the file may become corrupted. As an example the following cannot be used replacing C:\Program Files\Continuum\NewGraphicsFiles with E:\Graphics, but the following could replace C:\Program Files\Continuum\NewGraphicsFiles with E:\Program Files\Continuum\NewGraphicsFiles

 

Notes:

If a system is upgraded (new PCs) or a network drive that contains the image files is no longer available, then the graphics can be very slow to open.

Labels (1)
Labels:
  • Andover Continuum
Tags (2)
  • Find more articles tagged with:
  • 7844
  • DavidShore20
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.