Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Can current revision MNL family controllers be programmed with WorkPlace Tech release 4?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Can current revision MNL family controllers be programmed with WorkPlace Tech release 4?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa116868
    sesa116868
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1284 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Can current revision MNL family controllers be programmed with WorkPlace Tech release 4?

Picard Product_Support
‎2018-09-06 12:45 PM

Issue

Customer has previously purchased the WorkPlace Tech software release 4 and wants to know if there are any controllers available that can be programmed with the release 4.

Environment

WorkPlace Tech release 4.0

Existing MNL controllers of various releases.

Cause

WorkPlace Tech release 4.0 generates an error message when an existing application created for an old version of an MNL controller is downloaded into a new controller.

Resolution

See the section "Controller Firmware Revisions" in Chapter 1 of the WorkPlace Tech Tool 4.0 Engineering Guide for a explanation of the LON controller firmware versions.  If the controller application was programmed for use with an earlier version of the controller,  the application must be updated to the current version before the application can be downloaded into the controller.  Current production controllers contain revision 4.1 firmware.  The revision 4.1 controller model numbers are as follows:  MNL-5Rxx, MNL-10Rxx, MNL-15Rxx, MNL-20Rxx (where xx is F3, R3, H3 , S3 or S4), MNL-11RF3, MNL-13RF3 or MNL-VxRV3 (where x is 1, 2 or 3).    Older production controllers can be identified by the following model number series: MNL-10Rx1, MNL-20Rx1, MNL-VxRV1, MNL-5Rxx, MNL-10Rxx, MNL-15Rxx, MNL-20Rxx (where xx is F2, R2, H2 , S1 or S2), MNL-11RF2, MNL-13RF2 or MNL-VxRV2

To convert the application controller version, use the WorkPlace Tech "Hardware Wizard" after opening the application file.

  1. Open the Hardware Wizard.
  2. Click the [< Back] button at the bottom of the Hardware Wizard window to display the Controller Selection screen.
  3. Note that the current controller version for the application will be displayed in the box at the bottom of the window.
  4. If the old controller type is a MN V1, MN V2 or MN V3, select the [MN VAV] tab otherwise select the tab corresponding to the displayed controller type.
  5. On the controller selection page, select the model number of the new controller to be used for the application.  If the controllers are using the "Satellite" profile and the old controller was a "Satellite 1" profile, select the "Satellite 3" profile for the new controller.  Select "Satellite 4" if the old controller was a "Satellite 2" profile.  For all other controllers, select the new controller with the same profile type (Fan Coil, Heat Pump, Roof Top) as the original. 
  6. After selecting the controller profile for the replacement controller (in step 5), verify that the controller model number shown (MNL-xxxxx) matches the original controller, except for the last digit.  This is the model number of the controller that should be used for the replacement.
  7. Click the [Next] button to accept the new controller type selection then click the [Next] button to accept the controller configuration. Click the [Finish] button to exit the Hardware Wizard and apply the changes to the application.

The application can then be compiled and downloaded to the new controller.

Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 7195
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.